2.1 Creating a Libero Project
(Ask a Question)To create a Libero project, follow these steps:
- On the Libero menu bar, click
- Enter the following details, and click Next.
- Project name: PF_Mi_V_Tut
- Project location: For example, F:/Libero_Projects
- Preferred HDL type: Verilog
Figure 2-1. New Project Details
- To choose the PolarFire® device present on the PolarFire Evaluation Board, select the following settings in the Device Selection window, and click Next.
- Family: PolarFire
- Die: MPF300TS
- Package: FCG1152
- Speed: -1
- Range: IND
- Part Number: MPF300TS-1FCG1152I
Figure 2-2. Device Selection - In the Device Settings window, click Next to retain the default core voltage and I/O settings.
- In the Add HDL Sources window, click Next to retain the default settings.
- In the Add constraints window, click Import file to import the I/O constraint file.
- In the Import files
window, locate the
io_constraints.pdcfile in theDesignFiles_directory\HW\src\constraintsfolder, and double-click it. - Click Finish.
The Log pane displays a message indicating that the PF_Mi_V_Tut project was created.