3.6 Derived Output Quantities
Using Metrology module primary output quantities, the following quantities of interest (per-phase or system) may be derived, using the formulae indicated in the following sections.
Note: Care must be exercised when using RMS values with integrated values, depending on the
length of the integration period.