4.2.7 Super Capacitor
There is a 1x2, 100mil pin-header on the kit that can be used to connect/disconnect the super capacitor from the voltage backup system marked "SUPER CAP". The capacitor is connected by default with the jumper that is mounted on this pin-header. To disconnect the super capacitor remove the jumper.
| Pin | Function | Description |
|---|---|---|
| 1 | V_SUPERCAP | Connected directly to the positive pin of the capacitor |
| 2 | VBAT | VBAT input to the power switch |