3.5.4.1 Overview
The power amplifier of the ATA8510/15 works as a push-pull circuit according to the following figure. The current sources are switched between source and sink operation with the TX frequency, fTX.
After the fractional-N PLL is locked, the internal biasing of the power amplifier is
switched by using the RF front-end register FEEN2.PAEN = 1. This bit
setting enables the biasing of the block but not the current sources. The current
sources and the related RF carrier are switched on with the FSCR register after
FEEN2.PAEN = 1.
The tolerances of the current sources are calibrated with the RF front-end register FETN4.RTN4[3:0]. The calibration data is located in the factory-locked EEPROM and must be copied to the RF front-end register before activating the power amplifier.
The current source setting must be done in the RF front-end register, FEPAC, before activating the power amplifier.