1.1.11.5 WDRV_WINC_Tasks Function
void WDRV_WINC_Tasks(SYS_MODULE_OBJ object)
C
Summary
Maintains the WINC drivers state machine.
Description
This function is used to maintain the driver's internal state machine.
Precondition
WDRV_WINC_Initialize must have been called before calling this function.
Parameters
Param | Description |
object | Driver object handle, returned from WDRV_WINC_Initialize |
Returns
None.
Remarks
This function is normally not called directly by an application. It is called by the system's Tasks routine (SYS_Tasks).