1.1.10.3 WDRV_WINC_PowerSaveSetBeaconInterval Function
WDRV_WINC_STATUS WDRV_WINC_PowerSaveSetBeaconInterval (
DRV_HANDLE handle,
uint16_t numBeaconIntervals
)
C
Summary
Configures the beacon listening interval.
Description
The beacon listening interval specifies how many beacon period will occur between listening actions when the WINC is in low power mode.
Precondition
WDRV_WINC_Initialize should have been called. WDRV_WINC_Open should have been called to obtain a valid handle.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_WINC_Open. |
numBeaconIntervals | Number of beacon intervals between listening operations. |
Returns
WDRV_WINC_STATUS_OK - The interval has been accepted. WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open. WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect. WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
Remarks
None.