1.1.10.1 WDRV_WINC_PowerSaveGetMode Function
WDRV_WINC_PS_MODE WDRV_WINC_PowerSaveGetMode(DRV_HANDLE handle)
C
Summary
Returns the current power save mode.
Description
Returns to the caller the current power save mode in use by the WINC.
Precondition
WDRV_WINC_Initialize should have been called. WDRV_WINC_Open should have been called to obtain a valid handle.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_WINC_Open. |
Returns
WDRV_WINC_PS_MODE_INVALID - An error occurred.
Other WDRV_WINC_PS_MODE value - Current power save mode.
Remarks
None.