1.1.10.2 WDRV_WINC_PowerSaveManualSleep Function
WDRV_WINC_STATUS WDRV_WINC_PowerSaveManualSleep (
DRV_HANDLE handle, uint32_t sleepTime
)
C
Summary
Manual sleep power save operation.
Description
If the current power save mode is WDRV_WINC_PS_MODE_MANUAL the WINC can be placed into low power mode by requesting sleep.
Precondition
WDRV_WINC_Initialize should have been called. WDRV_WINC_Open should have been called to obtain a valid handle. Power save mode must be WDRV_WINC_PS_MODE_MANUAL
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_WINC_Open. |
sleepTime | Sleep period specified in milli-seconds. |
Returns
WDRV_WINC_STATUS_OK - The request has been accepted. WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open. WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect. WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
Remarks
None.