1.2.1.6 WDRV_PIC32MZW_Status Function
SYS_STATUS WDRV_PIC32MZW_Status(SYS_MODULE_OBJ object)
C
Summary
Provides the current status of the PIC32MZW driver module.
Description
This function provides the current status of the PIC32MZW driver module.
Precondition
WDRV_PIC32MZW_Initialize must have been called before calling this function.
Parameters
Param | Description |
object | Driver object handle, returned from WDRV_PIC32MZW_Initialize |
Returns
SYS_STATUS_READY - Indicates that any previous module operation for the specified module has completed SYS_STATUS_BUSY - Indicates that a previous module operation for the specified module has not yet completed SYS_STATUS_ERROR - Indicates that the specified module is in an error state
SYS_MODULE_OBJ object; // Returned from WDRV_PIC32MZW_Initialize
SYS_STATUS status;
status = WDRV_PIC32MZW_Status(object); if (SYS_STATUS_ERROR >= status)
{
// Handle error
}
Example
Remarks
Any value greater than SYS_STATUS_READY is also a normal running state in which the driver is ready to accept new operations. SYS_STATUS_BUSY - Indicates that the driver is busy with a previous system level operation and cannot start another SYS_STATUS_ERROR - Indicates that the driver is in an error state Any value less than SYS_STATUS_ERROR is also an error state.
SYS_MODULE_DEINITIALIZED - Indicates that the driver has been deinitialized This operation can
be used to determine when any of the driver's module level operations has completed. If the status operation returns SYS_STATUS_BUSY, then a previous operation has not yet completed. Once the status operation returns SYS_STATUS_READY, any previous operations have completed. The value of SYS_STATUS_ERROR is negative (-1). Any value less than that is also an error state. This function will NEVER block waiting for hardware. If the Status operation returns an error value, the error may be cleared by calling the reinitialize operation. If that fails, the deinitialize operation will need to be called, followed by the initialize operation to return to normal operations.