31.3.3.7 Conversion Timing

Some of the analog modules in the ADC are disabled between conversions and require time to initialize before the conversion starts. Only the modules used by the current ADC configuration are enabled, and since the initializations run in parallel, the limiting factor is the module with the slowest initialization time.

By writing the Low Latency (LOWLAT) bit in the Control A (ADCn.CTRLA) register to ‘1’, the latency of the ADC peripheral can be reduced. This will keep the configured modules continuously enabled, effectively removing all initialization time at the start of a conversion. Initialization time is still needed when enabling the ADC for the first time and reconfiguring the ADC to use an input or reference that requires initialization. The ADC Busy (ADCBUSY) bit in the Status (ADCn.STATUS) register can be used to check if initialization is ongoing.

The following table shows the initialization times required by the different analog modules.

Table 31-5. ADC Initialization Timing
Analog ModuleLOWLATInitialization Time (µs)
ADC010
1(1)0
Settling of internal references060
1(1)2(2)
Settling of internal references after changing from one internal reference voltage to anotherX35
Settling of external reference or VDD as the referenceX2
Settling of internal Temperature Sensor input060
1(1)0
Settling of internal Analog Comparator Reference DAC input035
1(1)0
Selecting VDD/10 as the inputX2
Note:
  1. The LOWLAT timing values are valid between two conversions that both have the LOWLAT bit written to ‘1’.
  2. When changing from one internal reference voltage to another internal reference voltage, the full 60 μs delay will be used if changing from a non-internal reference to an internal reference.

The sampling period of the input to the ADC is configured through the Sample Duration (SAMPDUR) bit field in the Control E (ADCn.CTRLE) register as SAMPDUR + 1 CLK_ADC cycles.