10.3 Sending Communication Packets

  1. Navigate to the Sender tab.
  2. Select a Packet Type from the drop-down in the toolbar.
  3. Click Add to create a new packet.
  4. Configure the packet fields (address, operation, data, etc.).
  5. Repeat steps 2–4 to add more packets as needed.
  6. Use the Up/Down arrows to reorder packets.
  7. Use the Enable/Disable toggle on each packet to include or exclude it from Send All.
  8. Click Send All to send all enabled packets in sequence, or click the individual Send button on a specific packet.
  9. Review the results using the send button state colors and the Details panel.