20.2.2 ETAP Data (ETAP_DATA)
Command
ETAP_DATA selects the Data register. The read/write Data
register is used for op code and data transfers during processor accesses.
The value read in the Data register is valid only if a processor access for
a write is pending, in which case the Data register holds the store value.
The value written to the Data register is only used if a processor access
for a pending read is finished afterwards; in which case, the data value
written is the value for the fetch or load. This behavior implies that the
Data register is not a memory location where a previously written value can
be read afterwards.