10.1 Four-Wire Interface
The following steps are required to enter Serial Execution mode:
Note: The assumption is that the MCLR pin
has been driven low from the previous check device status step (see Figure 8-1).
SendCommand (MTAP_SW_MTAP).- SetMode
(6’b011111). SendCommand (MTAP_COMMAND).- statusVal = XferData
(MCHP_STATUS). - If CPS (statusVal[7]) is not
‘
1’, first, erase the device. SendCommand (MTAP_SW_ETAP).- SetMode
(6’b011111). SendCommand (ETAP_EJTAGBOOT).- Set the MCLR pin high.