5.1 Programming Interface
Enhanced Tag Access Port (ETAP)
This block serially feeds instructions and data into the CPU.
Microchip Tag Access Port (MTAP)
In addition to the EJTAG TAP (ETAP) controller, the PIC32 device uses a second
proprietary TAP controller for additional operations. The Microchip TAP (MTAP)
controller supports two instructions relevant to programming,
MTAP_COMMAND and TAP switch instructions. See Table 20-1 for complete list of instructions. The
MTAP_COMMAND instruction provides a mechanism for a JTAG probe
to send commands to the device through its Data register.
The programmer sends commands by shifting in the MTAP_COMMAND
instruction through the SendCommand pseudo operation, and then
sending the MTAP_COMMAND DR commands through the
XferData pseudo operation, see Table 20-2 for specific commands. The probe does not need to issue an
MTAP_COMMAND instruction for every command shifted into the
Data register.
Two-Wire or Four-Wire
This block converts the Two-Wire ICSP™ interface to the Four-Wire JTAG interface.
CPU
The CPU executes instructions at 8 MHz through the internal oscillator.
Flash Controller
The Flash controller controls erasing and programming of the Flash memory on the device.
Flash Memory
The PIC32 device Flash memory is divided into two logical Flash partitions consisting of the Boot Flash Memory (BFM) and Program Flash Memory (PFM). The BFM begins at address 0x1FC00000, and the PFM begins at address 0x1D000000. Each Flash partition is divided into pages, which represent the smallest block of memory that can be erased. Depending on the device, page sizes are 256 words (1024 bytes), 1024 words (4096 bytes) or 4096 words (16,384 bytes). Row size indicates the number of words that are programmed with the row program command. There are always eight rows within a page; therefore, devices with 256, 1024 and 4096 word page sizes have 32, 128 and 512 word row sizes, respectively. Table 5-1 shows the PFM, BFM, row and page size of each device family.
For a PIC32MZ W1 device, the BFM begins at address 0x1FC00000, and the PFM begins at address 0x10000000. The Flash is divided into pages of 1024 words or 4-KB, which represents the smallest block of memory that can be erased. Row size indicates the number of words that are programmed with row program commands. The Flash contains four rows within a page with a total row size of 256 words or 1024 bytes.
Memory locations of the BFM are reserved for the device Configuration registers, see Configuration Memory and Device ID for more information.
| PIC32 Device | Row Size (Words) | Page Size (Words) | Boot Flash Memory Address (Bytes)(1) | Programming Executive(2, 3) |
|---|---|---|---|---|
| PIC32MX 110/120/130/150/170210/220/230/350/270 (28/36/44 pin devices only) | 32 | 256 | 0x1FC00000-0x1FC00BFF (3 KB) |
RIPE_11_aabbcc.hex
|
| PIC32MX 120/130/150/170/230/250/270/530/550/57 (64/100-pin devices only) | ||||
| PIC32MX 15X/17X/25X/27X (28/44-pin devices only) | 0x1FC00000-0x1FC02FFF (12 KB) | |||
| PIC32MZW1 10XX/20XX | 256 | 1024 | 0x1FC00000-0x1FC0FFFF (64 KB) | RIPE_25_aabbcc.hex |
| PIC32MX 330/350/370/430/450/470 | 128 | 1024 | 0x1FC00000-0x1FC02FFF (12 KB) | RIPE_06_aabbcc.hex |
| PIC32MX 320/340/360/420/440/460 | ||||
| PIC32MX 534/564/664/764 | ||||
| PIC32MX 575/675/695/795 | ||||
| PIC32MK 0512/1024XXD/E/F/K/L/M | 128 | 1024 |
| RIPE_15a_aabbcc.hex |
| PIC32MK 0256/0512XXG/H | 128 | 1024 | 0x1FC00000-0x1FC04FFF (20 KB) | RIPE_15a_aabbcc.hex |
| PIC32MZ 05XX/10XX/20XX | 512 | 4096 |
| RIPE_15_aabbcc.hex |
|
Note:
| ||||