Exiting programming mode is done by removing VIH from the MCLR pin, as illustrated in
Figure 16-1. The only requirement for exit is that an
interval, P16, must elapse between the last clock and program signals before removing
VIH.Figure 16-1. Four-Wire Exit Programming
Mode
The following steps are required to exit Programming mode:
SetMode (5’b11111).
Assert the MCLR pin.
Remove power (if the device is powered).
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.