1.2.4.4.6 SRV_PVDDMON_CALLBACK Typedef
C
typedef void (*SRV_PVDDMON_CALLBACK)( SRV_PVDDMON_CMP_MODE cmpMode, uintptr_t context );
Summary
Pointer to a PVDD Monitor Event handler function.
Description
This data type defines the required function signature for the PVDD Monitor Event handling callback function. A client must register a pointer using the callback register function whose function signature match the types specified by this function pointer in order to receive a notification related the comparison event.
Parameters
| Param | Description |
|---|---|
| cmpMode | Comparison mode - SRV_PVDDMON_CMP_MODE. |
| context | Pointer to parameters to be passed to Handler function. |
Returns
None.
Example
static void APP_PLC_PVDDMonitorCb( SRV_PVDDMON_CMP_MODE cmpMode, uintptr_t context )
{
(void)context;
if (cmpMode == SRV_PVDDMON_CMP_MODE_OUT)
{
/* PLC Transmission is not permitted */
DRV_PLC_PHY_EnableTX(appPlc.drvPl360Handle, false);
appPlc.pvddMonTxEnable = false;
/* Restart PVDD Monitor to check when VDD is within the comparison window */
SRV_PVDDMON_Restart(SRV_PVDDMON_CMP_MODE_IN);
}
else
{
/* PLC Transmission is permitted again */
DRV_PLC_PHY_EnableTX(appPlc.drvPl360Handle, true);
appPlc.pvddMonTxEnable = true;
/* Restart PVDD Monitor to check when VDD is out of the comparison window */
SRV_PVDDMON_Restart(SRV_PVDDMON_CMP_MODE_OUT);
}
}