1.2.4.4.4 SRV_PVDDMON_CallbackRegister Function

C

void SRV_PVDDMON_CallbackRegister
(
    SRV_PVDDMON_CALLBACK callback,
    uintptr_t context
);

Summary

Allows a client to identify a PVDD Monitor event handling function to call back when the PVDD level is in/out comparison window.

Description

The callback once set, persists until the client closes the sets another callback (which could be a NULL pointer to indicate no callback).

Parameters

ParamDescription
callbackPointer to the callback function.
contextThe value of parameter will be passed back to the client unchanged, when the callback function is called.

Returns

None.

Example

/* Enable PLC PVDD Monitor Service */
SRV_PVDDMON_CallbackRegister(APP_PLC_PVDDMonitorCb, 0);
/* Notify when PVDD level leaves the comparison window */
SRV_PVDDMON_Start(SRV_PVDDMON_CMP_MODE_OUT);

Remarks

None.