1.1.10.7 WDRV_WINC_BSSFindFirst
C
WDRV_WINC_STATUS WDRV_WINC_BSSFindFirst
(
DRV_HANDLE handle,
WDRV_WINC_CHANNEL_ID channel,
bool active,
const WDRV_WINC_SSID_LIST *const pSSIDList,
const WDRV_WINC_BSSFIND_NOTIFY_CALLBACK pfNotifyCallback
)Description
A scan is requested on the specified channels. An optional callback can be provided to receive notification of the first BSS discovered.
Precondition
WDRV_WINC_Initialize must have been called.
WDRV_WINC_Open must have been called to obtain a valid handle.
Parameters
| Parameters | Description |
|---|---|
| handle | Client handle obtained by a call to WDRV_WINC_Open. |
| channel | Channel to scan, maybe WDRV_WINC_ALL_CHANNELS or WDRV_WINC_CID_ANY in which case all enabled channels are scanned. |
| active | Use active vs passive scanning |
| pSSIDList | Pointer to list of SSIDs to match on. |
| pfNotifyCallback | Callback to receive notification of first BSS found. |
Returns
- WDRV_WINC_STATUS_OK - A scan was initiated.
- WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open.
- WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected.
- WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
- WDRV_WINC_STATUS_SCAN_IN_PROGRESS - A scan is already in progress.
Remarks
If channel is WDRV_WINC_ALL_CHANNELS or WDRV_WINC_CID_ANY then all enabled channels are scanned. The enabled channels can be configured using WDRV_WINC_BSSFindSetScanChannels24. How the scan is performed can be configured using WDRV_WINC_BSSFindSetScanParameters.
If active is false and pSSIDList is not NULL then the result is WDRV_WINC_STATUS_INVALID_ARG. Passive scan with an SSID List is not supported.