3.2.8.7.2 MQTT System Service Interface
This section describes the MQTT System Service Interface
MQTT Service Status Enum
States involved in the operation of the MQTT state
machine.
typedef enum
{
SYS_RNWF_MQTT_CONFIG, /**<Configure the MQTT Broker parameters*/
SYS_RNWF_MQTT_CONNECT, /**<Connect to the MQTT Broker */
SYS_RNWF_MQTT_RECONNECT, /**<Request reconnect to the MQTT Cloud*/
SYS_RNWF_MQTT_DISCONNECT, /**<Trigger Disconnect from MQTT Broker*/
SYS_RNWF_MQTT_SUBSCRIBE_QOS, /**<Subscribe to QoS Topics */
SYS_RNWF_MQTT_PUBLISH, /**<Publis to MQTT Broker*/
SYS_RNWF_MQTT_SET_CALLBACK, /**<Configure the MQTT Application Callback*/
}SYS_RNWF_MQTT_SERVICE_t;MQTT Event Enum
Events involved in the operation of the MQTT state
machine
typedef enum
{
SYS_RNWF_MQTT_CONNECTED, /**<Connected to MQTT broker event */
SYS_RNWF_MQTT_DISCONNECTED, /**<Disconnected from MQTT broker event*/
SYS_RNWF_MQTT_SUBCRIBE_MSG, /**<Event to report received MQTT message*/
}SYS_RNWF_MQTT_EVENT_t;MQTT Message Configuration Struct
Defines the configuration parameters required to establish connection
with MQTT Broker
typedef struct
{
/**<MQTT Broker/Server URL */
const char *url;
/**<MQTT Service client ID*/
const char *clientid;
/**<MQTT User Name Credential */
const char *username;
/**<MQTT Password Credential */
const char *password;
/**<MQTT Broker/Server Port */
uint16_t port;
/*MQTT TLS Index*/
uint8_t tls_idx;
/*Azure DPS*/
uint8_t azure_dps;
/*TLS Configuration*/
uint8_t *tls_conf;
/*MQTT Protocol Version*/
uint8_t protoVer;
/*MQTT Keep Alive time */
uint16_t keep_alive_time;
}SYS_RNWF_MQTT_CFG_t;MQTT Message Enum
typedef enum
{
SYS_RNWF_NEW_MSG, /**New message*/
SYS_RNWF_DUP_MSG /**Duplicate message*/
}SYS_RNWF_MQTT_MSG_t;
MQTT QoS Enum
typedef enum
{
SYS_RNWF_MQTT_QOS0, /**<No-Ack, Best effort delivery(No Guarantee)*/
SYS_RNWF_MQTT_QOS1, /**<Pub-Ack, sent untill PUBACK from broker(possible duplicates) */
SYS_RNWF_MQTT_QOS2, /**<Highest service, no duplicate with guarantee */
}SYS_RNWF_MQTT_QOS_t;
MQTT Publish Retain Enum
Sets whether the published message is retained at the broker or
not.
typedef enum
{
SYS_RNWF_NO_RETAIN, /**<Publish message is not saved at broker */
SYS_RNWF_RETAIN, /**<Publish message is saved at broker */
}SYS_RNWF_MQTT_RETAIN_t;MQTT Frame Struct
typedef struct
{
SYS_RNWF_MQTT_MSG_t isNew; /**<Indicates message is new or duplicate */
SYS_RNWF_MQTT_QOS_t qos; /**<QoS type for the message ::RNWF_MQTT_QOS_t */
SYS_RNWF_MQTT_RETAIN_t isRetain; /**<Retain flag for the publish message */
const uint8_t *topic; /**<Publish topic for the message */
const uint8_t *message; /**<Indicates message is new or duplicate */
}SYS_RNWF_MQTT_FRAME_t;
MQTT LWT Configuration Struct
typedef struct
{
/**<QoS type for the LWT message ::SYS_RNWF_MQTT_QOS_t */
SYS_RNWF_MQTT_QOS_t qos;
/**<Retain flag for the LWT message */
SYS_RNWF_MQTT_RETAIN_t isRetain;
/**<Topic name of the LWT message */
const char *topic_name;
/**<LWT message */
const char *message;
}SYS_RNWF_MQTT_LWT_CFG_t;