5.1.3 BLE Multirole Multilink Transparent UART

This section explains how to create a multirole multilink device and send/receive characters between connected BLE devices over Microchip proprietary Transparent UART Profile. The multilink central enables users to connect multiple peripheral devices to a central device. The multilink central device acts as peripheral device and is connected to an another central device(MBD application). The central is MBD application and peripheral devices in this tutorial are WBZ351 devices.

Users can choose to either run the precompiled Application Example hex file provided on the WBZ351 Curiosity Board or follow the steps to develop the application from scratch.

It is recommended to follow the examples in sequence to understand the basic concepts before progressing to the advanced topics.

Hardware Requirement

Table 5-34. Hardware Prerequisites
S. No.ToolQuantity
1WBZ351 Curiosity Board3 (min)
2Micro USB cable3

SDK Setup

Refer to Getting Started with Software Development from Related Links.

Software Requirement

To install Tera Term tool, refer to the Tera Term web page in Reference Documentation from Related Links.

Smartphone App

Light Blue

Programming the Precompiled Hex file or Application Example

Using MPLAB® X IPE:

  1. Import and program the precompiled hex file: <Discover Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\multirole\multilink\hex.
  2. For detailed steps, refer to Programming a Device in MPLAB® IPE in Reference Documentation from Related Links.
    Note: Ensure to choose the correct Device and Tool information.

Using MPLAB® X IDE:

  1. Perform the following the steps mentioned in Running a Precompiled Example. For more information, refer to Running a Precompiled Application Example from Related Links.
  2. Open and program the application mr_ml_trp_uart.x located in <Discover Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\multirole\multilink\firmware.
  3. For more details on how to find the Discover path, refer to Download Application Example from Discover in Running a Precompiled Application Example from Related Links.

Demo Description

Upon programming the demo application, multirole multilink device (WBZ351) will start scanning for near by peripheral devices to connect. After a connection has been made data can be sent back and forth over UART between the two devices that are connected. The multirole multilink device continues scanning until 100 secs and allows new peripheral devices that are advertising to join. For this example we are going to demonstrate 2 BLE links

Central Device → MultiRole MultiLink Device → Peripheral Device1 & Peripheral Device2 & Peripheral Device3

Demo will print start of the scanning “Scanning”,connected “Connected!” and disconnected “Disconnected” state on a terminal emulator like TeraTerm@ (Speed: 115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none) Application Data to be sent to the connected peripheral device should be entered in the terminal emulator.

Testing

Users must use four WBZ351 Curiosity boards.
Note: For demo testing with multiple links, users need to configure the BLE Device Address for the three peripheral devices as follows:
  • Device 1 will have PUBLIC address of {0xA1, 0xA2, 0xA3, 0xA4, 0xA5, 0xA6}
  • Device 2 will have PUBLIC address of {0xB1, 0xB2, 0xB3, 0xB4, 0xB5, 0xB6}
  • Device 3 will have PUBLIC address of {0xC1, 0xC2, 0xC3, 0xC4, 0xC5, 0xC6}

Precompiled Hex files for peripheral devices with different addresses as mentioned above are available here.

Demo Experience when using four WBZ351 Curiosity boards, three configured as Peripheral and one configured as MultiRole device This section assumes that a user has already programmed the peripheral_trp_uart application on three WBZ351 Curiosity Boards.

  • Board1 = WBZ351 Curiosity Board with mr_ml_trp_uart applicaton Programmed
  • Board2(Device1) = WBZ351 Curiosity Board with peripheral_trp_uart application Programmed
  • Board3(Device2) = WBZ351 Curiosity Board with peripheral_trp_uart application Programmed
  • Board4(Device3) = WBZ351 Curiosity Board with peripheral_trp_uart application Programmed
  • Phone1 = Smartphone with MBD app installed
Note: It is recommended to reset multirole multilink device first and then the peripheral devices one by one
  • Board1:
    • Open TeraTerm @ (Speed: 115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none).
    • Reset the board. Upon reset, “Scanning” message is displayed on the TeraTerm.
    • Upon finding peripheral device with public address {0xA1, 0xA2, 0xA3, 0xA4, 0xA5, 0xA6} message “Found Peer Node” will be displayed and a connection request will be initiated “Initiating connection”.
    • During the scan time if more devices are available which will be true in this case, multirole multilink device will keep initiating connections with the new peer nodes.
    • After the scan period, a “Scan Completed” message will be displayed and the device will begin advertising as a peripheral. Once advertisement starts, an “Advertising” message will display.
  • Board2/Board3/Board4:
    • Open TeraTerm @ (Speed: 115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none).
    • Reset the board. Upon reset, “Advertising” message is displayed on the TeraTerm.
      Note: Scanner is configured to scan only for 100 seconds. Ensure the peer device is advertising.
  • Phone1 MBD setup:

    • Select BLE UART
    • Select PIC32CXBZ
    • Select Start
    • Wait for the mr_ml_trp_uart device to complete its scanning and to start advertising, then select “pic32cx-bz” to connect
    • Select “Text mode”
    • Within the settings, ensure that “Display data” is turned ON
After connection has been established between all peripheral devices and the central MBD device, the TeraTerm windows will look like the image below and the MBD will look like the image below.
Users can now start sending data back and forth between the multirole multilink device and central/peripheral device using the terminal emulator and MBD.
  • Characters entered on multirole multilink device (Board1) terminal emulator will appear on peripheral devices (Board2,3,4) emulator in a round-robin fashion without priority. For example, typing “abc” in the multirole multilink device terminal emulator will print “a” on one peripheral terminal emulator, “b” on another peripheral terminal emulator, and “c” on the last peripheral terminal emulator as shown below
  • Characters entered on any peripheral devices (Board2,3,4) terminal emulator will appear on central device's (Board1) terminal emulator with the prefix “Client Data :” as shown below.
  • Characters entered on any central device (Phone1 with MBD app) using Rx char (49535343-8841-43f4-a8d4-ecbe34729bb3) will appear on multirole device's (Board1) terminal emulator and will be forwarded to the peripheral devices (Board2,3,4). Consequently, the message will be printed on the peripheral device’s terminal emulators. This data will have the prefix of “Server Data :” on the multirole multilink (Board1) terminal emulator To send data on MBD, select the “Input String” field, type a message, and press send
    If successful, the MBD screen will look like the image below and the TeraTerm windows will look like the image below.

Developing this Application from scratch using MPLAB Code Configurator

Follow the steps below to build the application manually:
Note: It is recommended for the new users of the MPLAB Code Configurator to refer MPLAB® Code Configurator (MCC) User’s Guide in Reference Documentation from Related Links.
  1. Create a new harmony project. For more details, see Creating a New MCC Harmony Project from Related Links.
  2. Import component configuration: This step helps users setup the basic components and configuration required to develop this application. For more details on importing the component configuration, refer to Importing Existing App Example Configuration from Related Links.
    Note: Import and Export functionality of component configuration will help users to start from a known working setup of configuration.
  3. Accept dependencies or satisfiers when prompted.
  4. Verify if the Project Graph window has all the expected configuration.
    Figure 5-201. Project Graph

Verify Scan, Advertisement and Transparent Profile Configuration

  1. Select BLE_Stack component in project graph.
    Note: Advertising Interval Min and Max can be modified. Advertisement payload can be configured by user here.
  2. Select Transparent Profile configuration.

Generating a Code

For more details on code generation, refer to MPLAB Code Configurator (MCC) Code Generation from Related Links.

Files and Routines Automatically Generated by the MCC

After generating the program source from MCC interface by clicking Generate Code, the BLE configuration can be found in the following project directories.
Initialization routines for OSAL, RF System, and BLE System are auto-generated by the MCC. See OSAL Libraries Help in Reference Documentation from Related Links. Initialization routine executed during program initialization can be found in the project files.
The BLE stack initialization routine executed during Application Initialization can be found in project files. This intitialization routine is automatically generated by the MCC. This call initializes and configures the GAP, GATT, SMP, L2CAP and BLE middleware layers.
During system sleep, clock (system PLL) will be disabled and system tick will be turned off. FreeRTOS timer needs to be componsated for the time spent in sleep. RTC timer which works in the sleep mode is used to accomplish this. RTC timer will be initialized after BLE stack initialization.
Table 5-35. Source Files
Source FilesUsage
app.cApplication State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations
app_ble.cSource Code for the BLE stack related component configurations, code related to function calls from app.c
app_ble_handler.cAll GAP, GATT, SMP and L2CAP Event handlers
app_trspc_handler.cAll Transparent UART Client related Event handlers
app_trsps_handler.cAll Transparent UART Server related Event handlers
ble_trspc.cAll Transparent Client Functions for user application
ble_trsps.cAll Transparent Server Functions for user application
Note: app.c is autogenerated and has a state machine based Application code sample and users can use this template to develop their application.

Header Files

  • ble_gap.h: This header file contains BLE GAP functions and is automatically included in the app.c file

  • ble_trspc.h: This is the header file associated with API’s and structures related to BLE Transparent Client functions for Application User

  • ble_trsps.hThis is the header file associated with API’s and structures related to BLE Transparent Server functions for Application User

Function Calls

  • MCC generates and adds the code to initialize the BLE Stack GAP, GATT, SMP and L2CAP in APP_BleStackInit()
  • APP_BleStackInit() is the API that will be called inside the Applications Initial State APP_STATE_INIT in app.c

User Application Development

Include
  • Include the user action. For more information, refer to User Action from Related Links.
  • ble_trspc.h in app.c, BLE Transparent UART client related API's are available here

  • ble_trsps.h in app.c, BLE Transparent UART Server related API's are available here

  • osal/osal_freertos_extend.h in app_trsps_handler.c, OSAL related API's are available here

  • definitions.h in all the files where UART will be used to print debug information
    Note: definitions.h is not specific to just UART peripheral, instead it should be included in all application source files where peripheral functionality will be exercised.
Start Scanning
BLE_GAP_SetScanningEnable(true, BLE_GAP_SCAN_FD_ENABLE, BLE_GAP_SCAN_MODE_OBSERVER, 1000);

This API is called in the Applications initialstate - APP_STATE_INIT in app.c. Scan duration is 100 seconds.

Scan Results and intiating a BLE Connection
  • BLE_GAP_EVT_ADV_REPORT event is generated upon finding Advertisements on legacy channels

  • BLE connection can be initiated by using the API BLE_GAP_CreateConnection(&createConnParam_t);
    // code snippet to filter scan results and initiate connection
      // Filter Devices based of Address, for this example address checking only 2 bytes
      if ((p_event->eventField.evtAdvReport.addr.addr[0] == 0xA1 && p_event->eventField.evtAdvReport.addr.addr[1] == 0xA2) ||
          (p_event->eventField.evtAdvReport.addr.addr[0] == 0xB1 && p_event->eventField.evtAdvReport.addr.addr[1] == 0xB2) ||
          (p_event->eventField.evtAdvReport.addr.addr[0] == 0xC1 && p_event->eventField.evtAdvReport.addr.addr[1] == 0xC2))
      {
          SERCOM0_USART_Write((uint8_t *)"Found Peer Node\r\n", 17);
          BLE_GAP_CreateConnParams_T createConnParam_t;
          createConnParam_t.scanInterval = 0x3C; // 37.5 ms
          createConnParam_t.scanWindow = 0x1E; // 18.75 ms
          createConnParam_t.filterPolicy = BLE_GAP_SCAN_FP_ACCEPT_ALL;
          createConnParam_t.peerAddr.addrType = p_event->eventField.evtAdvReport.addr.addrType;
          memcpy(createConnParam_t.peerAddr.addr, p_event->eventField.evtAdvReport.addr.addr, GAP_MAX_BD_ADDRESS_LEN);
          createConnParam_t.connParams.intervalMin = 0x10;
          createConnParam_t.connParams.intervalMax = 0x10;
          createConnParam_t.connParams.latency = 0;
          createConnParam_t.connParams.supervisionTimeout = 0x48;
          SERCOM0_USART_Write((uint8_t *)"Initiating Connection\r\n", 23);
          BLE_GAP_CreateConnection(&createConnParam_t);
      }
Connected & Disconnected Events
  • In app_ble_handler.c, BLE_GAP_EVT_CONNECTED event will be generated when a BLE connection is completed
Connection Handler
  • Connection handle associated with the peer peripheral device needs to be saved for data exchange after a BLE connection

  • p_event->eventField.evtConnect.connHandle has this information

  • In Multilink Application, unique connection handler's will be generated for all the peripheral links
Scan Timeout Handler
  • The initiated scan operation will provide scan timeout event, we can start the advertisement to connect with another central device
Transmit Data
  • Add APP_MSG_UART_CB to the generated APP_MsgId_T
  • BLE_TRSPC_SendData(conn_hdl[i], 1, &uart_data); is the API to be used for sending data towards the Client device
  • BLE_TRSPS_SendData(conn_hdl[i], 1, &uart_data); is the API to be used for sending data towards the Server device

    Note: * The precompiled application example uses a UART callback to initiate the data transmission upon receiving a character on UART.
    Example Implementation for transmitting the received data over UART using the BLE_TRSPC_SendData API
    uint16_t conn_hdl[3];// connection handle info captured @BLE_GAP_EVT_CONNECTED event
    uint8_t uart_data;
    uint8_t no_of_links;// No of connected peripheral devices
    uint8_t i = 0;// link index
    void uart_cb(SERCOM_USART_EVENT event, uintptr_t context)
    {
      APP_Msg_T   appMsg;   
      // If RX data from UART reached threshold (previously set to 1)
      if( event == SERCOM_USART_EVENT_READ_THRESHOLD_REACHED )
      {
        // Read 1 byte data from UART
        SERCOM0_USART_Read(&uart_data, 1);
     
        appMsg.msgId = APP_MSG_UART_CB;
        OSAL_QUEUE_Send(&appData.appQueue, &appMsg, 0);     
      }
    }
     
    void APP_UartCBHandler()
    {
        // Send the data from UART to connected device through Transparent service
        BLE_TRSPC_SendData(conn_hdl[i], 1, &uart_data);
        i++;
        if(i==no_of_links) i = 0; //reset link index    
    }
     
      // Register call back when data is available on UART for Peripheral Device to send
      // Enable UART Read
      SERCOM0_USART_ReadNotificationEnable(true, true);
      // Set UART RX notification threshold to be 1
      SERCOM0_USART_ReadThresholdSet(1);
      // Register the UART RX callback function
      SERCOM0_USART_ReadCallbackRegister(uart_cb, (uintptr_t)NULL);
Receive Data
  • BLE_TRSPC_EVT_RECEIVE_DATA is the event generated when data is sent from peripheral device

  • Users need to use the BLE_TRSPC_GetDataLength(&data_len) & BLE_TRSPS_GetDataLength(&data_len) API to extract the length of application data received

  • BLE_TRSPC_GetData(&conn_hdl, data); & BLE_TRSPS_GetData(&conn_hdl, data); API is used to retrieve the data, conn_hdl is the value obtained from Connection Handler section
    Note:
    1. BLE_TRSPC_Event_T p_event structure stores the information about BLE transparent UART callback functions
    2. BLE_TRSPS_Event_T p_event structure stores the information about BLE transparent UART callback functions
    Example Implementation for printing the received data from peripheral device over UART
                /* TODO: implement your application code.*/
                uint16_t data_len;
                uint8_t *data;
                // Retrieve received data length
                BLE_TRSPC_GetDataLength(p_event->eventField.onReceiveData.connHandle, &data_len);
                // Allocate memory according to data length
                data = OSAL_Malloc(data_len);
                if(data == NULL)
                break;
                // Retrieve received data
                BLE_TRSPC_GetData(p_event->eventField.onReceiveData.connHandle, data);
                // Output received data to UART
                SERCOM0_USART_Write((uint8_t *)"\r\nClient Data :", 15);
                SERCOM0_USART_Write(data, data_len);
                // Free memory
                OSAL_Free(data);
Note: Users can explore more BLE Advertisement functionalities using the BLE Stack APIs. For more information, refer to BLE Stack in Reference Documentation from Related Links.