5.1.2.11 Path Loss Feature in Legacy Advertisements

This section explains how to enable the Path Loss feature with BLE Advertisements on WBZ351 Curiosity board using the MPLAB Code Configurator(MCC)

The path loss is defined as the difference between the remote transmit power level and the average local RSSI measurement for the connection. In other words, Path loss refers to the attenuation or reduction in signal strength as it travels through the wireless channel from the transmitter (BLE device) to the receiver.

Path loss monitoring is a crucial feature in BLE, allowing for real-time assessment of signal strength and providing valuable insights for connection management.

Users can choose to either run the precompiled Application Example hex file provided on the WBZ351 Curiosity Board or follow the steps to develop the application from scratch.

It is recommended to follow the examples in sequence to understand the basic concepts before progressing to the advanced topics.

Understanding Path Loss

Path Loss Zones

BLE path loss monitoring divides signal strength into specific zones to facilitate effective management. The core path loss zones are:

  1. Low Zone
  2. Middle Zone
  3. High Zone

The BLE Controller continuously evaluates path loss and notifies the Host when it transitions between these zones, based on predefined boundaries.

Calculating Path Loss

Path loss is determined as the difference between the remote transmit power level (the power at which the remote BLE device transmits) and the average local Received Signal Strength Indication (RSSI) measurement for the connection.

Zone Transition Criteria

Path loss is considered to have entered a new zone under specific conditions:
  • Transition to a Higher Zone: Path loss becomes greater than or equal to the upwards boundary when moving to a higher zone.
  • Transition to a Lower Zone: Path loss becomes less than or equal to the downwards boundary when moving to a lower zone.

To prevent frequent zone switching, some hysteresis is provided. The upwards boundary should be greater than or equal to the downwards boundary, ensuring a smooth transition.

Correlation with Distance:

Path loss often correlates with the distance between BLE devices. A higher zone may indicate that the peer BLE device has moved farther away. This information can be invaluable for various applications, such as proximity detection and device localization.

Path Loss Measurement

Path loss monitoring relies on obtaining data about both the remote transmit power level and local RSSI measurements. Two procedures are commonly used for this purpose:
  • Power Control Request Procedure

    The Power Control Request procedure involves periodically requesting the remote BLE device to provide its transmit power level. Combining this information with local RSSI measurements enables the calculation of path loss.

  • Power Change Indication Procedure

    The Power Change Indication procedure informs the Controller when the remote BLE device changes its transmit power level. This can occur due to adaptive power management or other factors. Upon receiving a power change indication, the Controller updates its path loss calculations accordingly.

Power Control Request procedure in context of path loss monitoring

The Power Control Request procedure is a critical component of path loss monitoring in Bluetooth Low Energy (BLE). This procedure enables the measurement of the remote transmit power level, which is essential for calculating path loss accurately.

Practical Applications

Path loss monitoring in BLE finds applications in various scenarios:
  • Proximity Detection: Path loss data can be used to estimate the distance between BLE devices accurately. This is especially useful for applications such as asset tracking, location-based services, and contact tracing.
  • Adaptive Power Management: Knowledge of path loss allows the Controller to dynamically adjust the transmit power level. This optimization helps conserve energy while maintaining a stable connection.
  • Connection Maintenance: Path loss notifications serve as early warnings of degrading connections due to increasing path loss. This can trigger actions like reconfiguration or re-establishment of the connection to maintain service quality.
  • Interference Mitigation: In environments with substantial interference, path loss monitoring helps identify deteriorating signal quality. This early detection enables the implementation of countermeasures, such as channel hopping or adjusting transmission parameters.

Hardware Requirement

Table 5-32. Hardware Prerequisites
S. No. Tool Quantity
1WBZ351 Curiosity Board2
2Micro USB cable2

SDK Setup

Refer to Getting Started with Software Development from Related Links.

Software Requirement

To install Tera Term tool, refer to the Tera Term web page in Reference Documentation from Related Links.

Smartphone App

None

Programming the Precompiled Hex File or Application Example

Using MPLAB® X IPE:

  1. Import and program the Precompiled Hex file: <Discover Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\peripheral\Legacy_ADV_Pathloss\hex\Legacy_ADV_Pathloss.X.production.signed.hex.

  2. Import and program the Precompiled Hex file: <Discover Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\central\central_conn\hex\central_conn.X.production.signed.hex.

  3. For detailed steps, refer to Programming a Device in MPLAB® IPE in Reference Documentation from Related Links.
    Note: Ensure to choose the correct Device and Tool information.

Using MPLAB® X IDE:

  1. Perform the following the steps mentioned in Running a Precompiled Example. For more information, refer to Running a Precompiled Application Example from Related Links.
  2. Open and program the application: <Discover Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\peripheral\Legacy_ADV_Pathloss\firmware\Legacy_ADV_Pathloss.X.

  3. Open and program the application: <Discover Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\central\central_conn\firmware\central_conn.X.
  4. For more details on how to find the Discover path, refer to Download Application Example from Discover in Running a Precompiled Application Example from Related Links.

Demo Description

This application implements the path loss feature into a peripheral legacy advertisement application. The testing of this application is done by connecting the path loss feature included in the peripheral legacy application to a central connection application. After a successful connection, in the peripheral application serial console, the path loss and zone will be updated frequently.

Testing

  1. Using micro USB cables, connect the Debug USB on the Curiosity boards to a PC.
  2. Program the precompiled hex files or application examples as mentioned.
    Note: One WBZ351 board must be programmed with the path loss peripheral legacy advertisement application and the other board with the central connection application, see BLE Connection from Related Links.
    1. The board programmed with the central connection application, once booted, will start scanning and upon finding the device with BT Address A6A5A4A3A2A1, will initiate a connection.
  3. Open the Tera Term of the board programmed with the path loss peripheral legacy advertisement application and set the “Serial Port” to USB Serial Device and “Speed” to 115200. Press SW1 to reset the board. Upon reset, “Advertising” must be displayed in Tera Term.
    For more details on how to set the “Serial Port” and “Speed”, refer to COM Port Setup in Running a Precompiled Application Example from Related Links.
  4. Open the Tera Term of the board programmed with the central connection application and set the “Serial Port” to USB Serial Device and “Speed” to 115200. Press SW1 to reset the board. Upon reset, the following should be displayed in the terminal windows of the central and peripheral applications, respectively.

Developing the Application from Scratch using MPLAB Code Configurator

The path loss feature can be incorporated to any of the peripheral or central applications. Here, the path loss feature is showcased by implementing it in the peripheral advertisement application as a reference. Then, the path loss feature implemented in the peripheral legacy advertisement is tested by connecting it with the central connection application.

Follow the steps below to build the application manually:
Note: It is recommended for the new users of the MPLAB Code Configurator to refer MPLAB® Code Configurator (MCC) User’s Guide in Reference Documentation from Related Links.
  1. Create a new harmony project. For more details, see Creating a New MCC Harmony Project from Related Links.
  2. To setup the basic components and configuration required to develop this application, import component configuration. Import and Export functionality of the Harmony component configuration will help users to start from a known working setup of the MCC configuration. For more details on importing the component configuration, refer to Importing Existing App Example Configuration from Related Links.

  3. Accept dependencies or satisfiers when prompted.

  4. Verify if the Project Graph window has all the expected configuration.
    Figure 5-198. Project Graph

Generating a Code

For more details on code generation, refer to MPLAB Code Configurator (MCC) Code Generation from Related Links.

Files and Routines Automatically generated by the MCC

After generating the program source from the MCC interface by clicking Generate Code, the BLE configuration source and header files can then be found in the following project directories.

Initialization routines for OSAL, RF System, and BLE System are auto-generated by the MCC. See OSAL Libraries Help in Reference Documentation from Related Links. Initialization routine executed during program initialization can be found in the project file.

The BLE stack initialization routine executed during Application Initialization can be found in project files. This initialization routine is automatically generated by the MCC. This call initializes and configures the GAP, GATT, SMP, L2CAP and BLE middleware layers.

During system sleep, clock (system PLL) will be disabled and system tick will be turned off. FreeRTOS timer needs to be compensated for the time spent in sleep. RTC timer which works in sleep mode is used to accomplish this. RTC timer will be initialized after BLE stack initialization.

Figure 5-199. 
Autogenerated, Advertisement Data Format
Figure 5-200. AD Structures and Types
Table 5-33. Source Files
Source Files Usage
app.cApplication State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations
app_ble.cSource Code for the BLE stack related component configurations, code related to function calls from app.c
app_ble_handler.cAll GAP, GATT, SMP and L2CAP Event handlers
Note: app.c is autogenerated and has a state machine-based application code sample. Users can use this template to develop their own application. |

Header Files

  • ble_gap.h contains BLE GAP functions and is automatically included in app.c

Function Calls

  • MCC generates and adds the code to initialize the BLE Stack GAP, GATT, SMP and L2CAP in APP_BleStackInit()
  • APP_BleStackInit() is the API that will be called inside the Applications Initial State APP_STATE_INIT in app.c

User Application Development

Include

  • Include the user action. For more information, refer to User Action from Related Links.
  • definitions.h must be included in all the files where UART will be used to print debug information.
    Note: definitions.h is not specific to just UART but instead must be included in all the application source files where any peripheral functionality will be exercised.

Set PUBLIC Device Address in app_ble.c

  • BLE_GAP_SetDeviceAddr(&devAddr);

This API can be called in APP_BleConfig() located in file app_ble.c.

    BLE_GAP_Addr_T devAddr;
    devAddr.addrType = BLE_GAP_ADDR_TYPE_PUBLIC;
    devAddr.addr[0] = 0xA1;
    devAddr.addr[1] = 0xA2;
    devAddr.addr[2] = 0xA3;
    devAddr.addr[3] = 0xA4;
    devAddr.addr[4] = 0xA5;
    devAddr.addr[5] = 0xA6;

    // Configure device address
    BLE_GAP_SetDeviceAddr(&devAddr);

Start Advertisement in app.c

  • BLE_GAP_SetAdvEnable(0x01, 0);

This API is called in the Applications initialstate - APP_STATE_INIT in app.c.

Note: Users can explore more BLE functionalities using the BLE Stack APIs. For more information, refer to BLE Stack in Reference Documentation from Related Links.

Path Loss Configuration

Initially create two new enum to effectively handle the callback between the application layer and BLE stack.

In the app_ble_handler.c file:

The path loss configuration is enabled after a successful connection establishment. The steps required to enable the path loss feature begin with the reception of the connected event (BLE_GAP_EVT_CONNECTED) in the app_ble_handler.c file.

Upon receiving the connection event, control is passed from the BLE Stack to the application layer using a queue mechanism with a specific message ID, namely APP_MSG_CONNECT_CB.

In the application layer under service tasks:

Upon receiving the APP_MSG_CONNECT_CB message, the path loss configurations, including the connection handle, threshold, hysteresis, and minimum time spent, are set.

The BLE_GAP_SetPathLossReportingParams function is called, and the earlier set path loss configurations are passed as parameters. It is recommended to wait until this function call returns with a success event.

Upon receiving the success event, a new message is initiated via the queue with the message ID set as APP_MSG_PATHLOSS_CB. Subsequently, the path loss reporting enable function is initiated with the connection handle as a parameter.

In the Path Loss Event Handler (BLE_GAP_EVT_PATH_LOSS_THRESHOLD):

Within the Path Loss Event Handler, include the following code to gather information about the path loss and determine the current zone that the device has entered. This data is then displayed on the console or printed to an output.

Note: It has been observed that the Received Signal Strength Indicator (RSSI) readings may not accurately reflect the actual received power from a connected peer device when the incoming power level is approximately -50 dBm or higher.

Where to Go from Here

See BLE Connection from Related Links.