DecoderEventHandlerCB Function Pointer
C
typedef void (*DecoderEventHandlerCB)(uint32_t event, void *cb_param, void *ctxt);
Summary
DecoderEventHandlerCB - The Callback function template for the application defined callback Functions.
This will be passed from application in the form of FLAC_DEC_APPLICATIONCB_SET.
Description
FLAC decoder event handler callback
Precondition
Successful Registration via function FLAC_RegisterDecoderEventHandlerCallback by application
Parameters
event - The specific event that causes the callback
cb_param - Pointer to a callback specific parameter
ctxt - User defined pointer to a context set during the event registration, to be invoked upon callback
Returns
None
Remarks
None