10.1.3 Enable Function
Once the host descriptor has been initialized and the application callbacks have been set, the PL360 Host Controller must be enabled using the following function:
atpl360_res_t atpl360_enable(uint32_t ul_binary_address, uint32_t ul_binary_len);Parameters:
| ul_binary_address | Memory address where the PL360 firmware binary file is located |
| ul_binary_len | Size of the PL360 firmware binary file |
This function performs the following actions:
- Disable PLC interrupt
- Transfer firmware binary file to the PL360 device
- Check firmware integrity
- Enable PLC interrupt