3.3.2 User-Configurable LEDs
Two user-configurable LEDs are provided in this board. The following table provides details about the list of LEDs that the user can turn ON or OFF while using the connected GPIO pins.
Two user-configurable LEDs are provided in this board. The following table provides details about the list of LEDs that the user can turn ON or OFF while using the connected GPIO pins.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.