8.13.2 Set Transmit Power
The user can control the Tx power of ATWILC1000 or ATWILC3000 using the iw tool with the following command line arguments.
$ iw dev wlan0 set txpower fixed x
Where x is the desired Tx level in mBm (1dBm = 100mBm).
The supported levels are 0, 300, 600, 900, 1200, 1500, and 1800.
Note: If the input Tx power value is other
than the mentioned supported levels, the
x value is automatically set
to the first greater value.