8.13.10 Set Current Regulatory Domain
To get a list of identified APs with associated attributes such as like bssid, frequency, RSSI, encryption and SSID, use the following command:
$ iw reg set US
cfg80211: Calling CRDA for country: US
[root@buildroot ~]# cfg80211: Regulatory domain changed to country: US
cfg80211: DFS Master region: unset
cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 3000 mBm), (N/A)
cfg80211: (5170000 KHz - 5250000 KHz @ 80000 KHz), (N/A, 1700 mBm), (N/A)
cfg80211: (5250000 KHz - 5330000 KHz @ 80000 KHz), (N/A, 2300 mBm), (0 s)
cfg80211: (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 3000 mBm), (N/A)
cfg80211: (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 4000 mBm), (N/A)
To change the default regulatory domain that Linux uses at startup, the user
must edit the configuration file that was passed while starting the
wpa_cli using the vi tool. The configuration is as follows:
$ vi /etc/wilc_wpa_supplicant.conf
ctrl_interface=/var/run/wpa_supplicant
update_config=1
country=US
network={
ssid="AndroidAP"
key_mgmt=NONE
}