5.9 Unexpected Shoot-through with dVDS/dt

Unwanted MOSFET turn-ON, caused by CGD × dVDS/dt (see Figure 5-9) is often the cause of unexplained shoot through in the halfbridge circuit. Depending on the ratio of the CGS/CGD, when the dVDS/dt across low side MOSFET (Q2) occurs (i.e when high side MOSFET turns ON), there can be a voltage applied to the gate of the Q2 MOSFET, turning ON Q2, and causing shoot through. In effect, a gate bouncing occurs causing a ringing on the VS line and the power ground.

Figure 5-9. Unexpected Shoot Through With dVDS/dt

Considering Figure 5-9

I G D = C G D × d V D S / d t

IGD will flow towards the resistive load (and small inductive due to parasitics) of the gate driver and the CGS of the MOSFET. Hence, this unwanted condition may be minimized by looking at the Ciss/Cres in the MOSFET datasheet (Ciss/Cres gives an indication of CGS/ CGD); having a Ciss/Cres as large as possible will minimize this phenomenon. Also, an external capacitor can be added to the gate-source of the MOSFET (for example 1 nF), which will increase CGS/CGD.