16.2.6 RAM1K18
(Ask a Question)The RAM1K18 block contains 18,432 memory bits and is a true dual-port memory. It can also be configured in two-port mode. All read/write operations to the RAM1K18 memory are synchronous. To improve the read data delay, an optional pipeline register at the output is available. A feed-through write mode is also available to enable immediate access to the write data. The RAM1K18 memory has two data ports, which can be independently configured in any combination as follows:
- Dual-Port RAM with the following configurations:
- 1Kx18, 1Kx16
- 2Kx9, 2Kx8
- 4Kx4
- 8Kx2
- 16Kx1
- Two-Port RAM with the following configurations:
- 512x36, 512x32
- 1Kx18, 1Kx16
- 2Kx9, 2Kx8
- 4Kx4
- 8Kx2
- 16Kx1
The main features of the RAM1K18 memory block are as follows:
- It has 18,432 bits.
- It provides two independent data ports A and B.
- It has a true dual-port mode, for which both ports have word widths less than or equal to 18 bits.
- In true dual-port mode, each port can be independently configured to any of the following depth/width: 1Kx18, 1Kx16, 2Kx9, 2Kx8, 4Kx4, 8Kx2, and 16Kx1.
- The widths of each port can be different, but one needs to be a
multiple of the other. There are 29 unique combinations of true dual-port aspect
ratios:
- 1Kx18/1Kx18, 1Kx18/2Kx9
- 1Kx16/1Kx16, 1Kx16/2Kx8, 1Kx16/4Kx4, 1Kx16/8Kx2, 1Kx16/16Kx1
- 2Kx9/1Kx18, 2Kx9/2Kx9
- 2Kx8/1Kx16, 2Kx8/2Kx8, 2Kx8/4Kx4, 2Kx8/8Kx2, 2Kx8/16Kx1
- 4Kx4/1Kx16, 4Kx4/2Kx8, 4Kx4/4Kx4, 4Kx4/8Kx2, 4Kx4/16Kx1
- 8Kx2/1Kx16, 8Kx2/2Kx8, 8Kx2/4Kx4, 8Kx2/8Kx2, 8Kx2/16Kx1
- 16Kx1/1Kx16, 16Kx1/2Kx8, 16Kx1/4Kx4, 16Kx1/8Kx2, 16Kx1/16Kx1
- RAM1K18 also has a two-port mode. In this case, Port A becomes the read port and Port B becomes the write port.
- In two-port mode, each port can be independently configured to any of the following depth/width: 512x36, 512x32, 1Kx18, 1Kx16, 2Kx9, 2Kx8, 4Kx4, 8Kx2 and 16Kx1.
- The widths of each port can be different, but one needs to be a
multiple of the other. There are 45 unique combinations of two-port aspect
ratios:
- 512x36/512x36, 512x36/1Kx18, 512x36/2Kx9
- 512x32/512x32, 512x32/1Kx16, 512x32/2Kx8, 512x32/4Kx4, 512x32/8Kx2, 512x32/16Kx1
- 1Kx18/512x36, 1Kx18/1Kx18, 1Kx18/2Kx9
- 1Kx16/512x32, 1Kx16/1Kx16, 1Kx16/2Kx8, 1Kx16/4Kx4, 1Kx16/8Kx2, 1Kx16/16Kx1
- 2Kx9/512x36, 2Kx9/1Kx18, 2Kx9/2Kx9
- 2Kx8/512x32, 2Kx8/1Kx16, 2Kx8/2Kx8, 2Kx8/4Kx4, 2Kx8/8Kx2, 2Kx8/16Kx1
- 4Kx4/512x32, 4Kx4/1Kx16, 4Kx4/2Kx8, 4Kx4/4Kx4, 4Kx4/8Kx2, 4Kx4/16Kx1
- 8Kx2/512x32, 8Kx2/1Kx16, 8Kx2/2Kx8, 8Kx2/4Kx4, 8Kx2/8Kx2, 8Kx2/16Kx1
- 16Kx1/512x32, 16Kx1/1Kx16, 16Kx1/2Kx8, 16Kx1/4Kx4, 16Kx1/8Kx2, 16Kx1/16Kx1
- RAM1K18 performs synchronous operation for setting up the address as well as writing and reading the data. The address, data, block port select, and write enable inputs are registered.
- An optional pipeline register with a separate enable, synchronous-reset, and asynchronous-reset is available at the read data port to improve the clock-to-out delay.
- There is an independent clock for each port. The memory is triggered at the rising edge of the clock.
- The true dual-port mode supports an optional feed-through write mode, where the write data also appears on the corresponding read data port.
- Read from both ports at the same location is allowed.
- Read and write on the same location at the same time results in unknown data to be read. There is no collision prevention or detection. However, correct data are expected to be written into the memory.
The following table shows a simplified block diagram of the RAM1K18 memory block and gives the port descriptions.
Pin Name | Pin Direction | Type | Description | Polarity |
---|---|---|---|---|
A_ADDR[13:0] | Input | Dynamic | Port A address | — |
A_BLK[2:0] | Input | Dynamic | Port A block selects | High |
A_CLK | Input | Dynamic | Port A clock | Rising |
A_DIN[17:0] | Input | Dynamic | Port A write data | — |
A_DOUT[17:0] | Output | Dynamic | Port A read data | — |
A_WEN[1:0] | Input | Dynamic | Port A write enables (per byte) | High |
A_WIDTH[2:0] | Input | Static | Port A width/depth mode select | — |
A_WMODE | Input | Static | Port A feed-through write select | High |
A_ARST_N | Input | Dynamic | Port A reset (must be tied to 1) | Low |
A_DOUT_LAT | Input | Static | Port A pipeline register select | Low |
A_DOUT_ARST_N | Input | Dynamic | Port A pipeline register asynchronous reset | Low |
A_DOUT_CLK | Input | Dynamic | Port A pipeline register clock (must be tied to A_CLK or 1) | Rising |
A_DOUT_EN | Input | Dynamic | Port A pipeline register enable | High |
A_DOUT_SRST_N | Input | Dynamic | Port A pipeline register synchronous reset | Low |
B_ADDR[13:0] | Input | Dynamic | Port B address | — |
B_BLK[2:0] | Input | Dynamic | Port B block selects | High |
B_CLK | Input | Dynamic | Port B clock | Rising |
B_DIN[17:0] | Input | Dynamic | Port B write data | — |
B_DOUT[17:0] | Output | Dynamic | Port B read data | — |
B_WEN[1:0] | Input | Dynamic | Port B write enables (per byte) | High |
B_WIDTH[2:0] | Input | Static | Port B width/depth mode select | — |
B_WMODE | Input | Static | Port B Feed-through write select | High |
B_ARST_N | Input | Dynamic | Port B reset (must be tied to 1) | Low |
B_DOUT_LAT | Input | Static | Port B pipeline register select | Low |
B_DOUT_ARST_N | Input | Dynamic | Port B pipeline register asynchronous reset | Low |
B_DOUT_CLK | Input | Dynamic | Port B pipeline register clock (must be tied to B_CLK or 1) | Rising |
B_DOUT_EN | Input | Dynamic | Port B pipeline register enable | High |
B_DOUT_SRST_N | Input | Dynamic | Port B pipeline register synchronous reset | Low |
A_EN | Input | Static | Port A power-down (must be tied to 1) | Low |
B_EN | Input | Static | Port B power-down (must be tied to 1) | Low |
SII_LOCK | Input | Static | Lock access to SII | High |
BUSY | Output | Dynamic | Busy signal from SII | High |
Signal Descriptions for RAM1K18
A_WIDTH AND B_WIDTH
The following table lists the width/depth mode selections for each port. Two-port mode is in effect when the width of at least one port is 36, and A_WIDTH indicates the read width while B_WIDTH indicates the write width. Also, when the write width is 36, the read width must also be 36.
Depth x Width | A_WIDTH/B_WIDTH |
---|---|
16Kx1 | 000 |
8Kx2 | 001 |
4Kx4 | 010 |
2Kx8, 2Kx9 | 011 |
1Kx16, 1Kx18 | 100 |
512x32, 512x36 (Two-port) |
101 11x |
A_WEN AND B_WEN
The following table lists the write/read control signals for each port. Two-port mode is in effect when the width of at least one port is 36, and read operation is always enabled. Also, when the write width is 36, both A_WEN and B_WEN must be static.
Depth x Width | A_WEN/B_WEN | Result |
---|---|---|
16Kx1, 8Kx2, 4Kx4, 2Kx8, 2Kx9, 1Kx16, 1Kx18 | 00 | Perform a read operation |
16Kx1, 8Kx2, 4Kx4, 2Kx8, 2Kx9 | 01 | Perform a write operation |
1Kx16 | 01 | Write [7:0] |
10 | Write [16:9] | |
11 | Write [16:9], [7:0] | |
1Kx18 | 01 | Write [8:0] |
10 | Write [17:9] | |
11 | Write [17:0] | |
512x32 (Two-port write) |
B_WEN[0] = 1 | Write B_DIN[7:0] |
B_WEN[1] = 1 | Write B_DIN[16:9] | |
A_WEN[0] = 1 | Write A_DIN[7:0] | |
A_WEN[1] = 1 | Write A_DIN[16:9] | |
512x36 (Two-port write) |
B_WEN[0] = 1 | Write B_DIN[8:0] |
B_WEN[1] = 1 | Write B_DIN[17:9] | |
A_WEN[0] = 1 | Write A_DIN[8:0] | |
A_WEN[1] = 1 | Write A_DIN[17:9] |
A_ADDR AND B_ADDR
The following table address buses for the two ports. Fourteen bits are needed to address the 16K independent locations in x1 mode. In wider modes, fewer address bits are used. The required bits are MSB justified and unused LSB bits must be tied to 0. A_ADDR is synchronized by A_CLK while B_ADDR is synchronized to B_CLK. Two-port mode is in effect when the width of at least one port is 36, and A_ADDR provides the read address while B_ADDR provides the write address.
Depth x Width | A_ADDR/B_ADDR | |
---|---|---|
Used Bits | Unused Bits (must be tied to 0) |
|
16Kx1 | [13:0] | None |
8Kx2 | [13:1] | [0] |
4Kx4 | [13:2] | [1:0] |
2Kx8, 2Kx9 | [13:3] | [2:0] |
1Kx16, 1Kx18 | [13:4] | [3:0] |
512x32, 512x36 (Two-port) |
[13:5] | [4:0] |
A_DIN AND B_DIN
The following table lists the data input buses for the two ports. The required bits are LSB justified and unused MSB bits must be tied to 0. Two-port mode is in effect when the width of at least one port is 36, and A_DIN provides the MSB of the write data while B_DIN provides the LSB of the write data.
Depth x Width | A_DIN/B_DIN | |
---|---|---|
Used Bits | Unused Bits (must be tied to 0) |
|
16Kx1 | [0] | [17:1] |
8Kx2 | [1:0] | [17:2] |
4Kx4 | [3:0] | [17:4] |
2Kx8 | [7:0] | [17:8] |
2Kx9 | [8:0] | [17:9] |
1Kx16 | [16:9] is [15:8] [7:0] is [7:0] |
[17] [8] |
1Kx18 | [17:0] | None |
512x32 (Two-port write) |
A_DIN[16:9] is [31:24] A_DIN[7:0] is [23:16] B_DIN[16:9] is [15:8] B_DIN[7:0] is [7:0] |
A_DIN[17] A_DIN[8] B_DIN[17] B_DIN[8] |
512x36 (Two-port write) |
A_DIN[17:0] is [35:18] B_DIN[17:0] is [17:0] |
None |
A_DOUT AND B_DOUT
The following table lists the data output buses for the two ports. The required bits are LSB justified. Two-port mode is in effect when the width of at least one port is 36, and A_DOUT provides the MSB of the read data while B_DOUT provides the LSB of the read data.
Depth x Width | A_DOUT/B_DOUT | |
---|---|---|
Used Bits | Unused Bits | |
16Kx1 | [0] | [17:1] |
8Kx2 | [1:0] | [17:2] |
4Kx4 | [3:0] | [17:4] |
2Kx8 | [7:0] | [17:8] |
2Kx9 | [8:0] | [17:9] |
1Kx16 | [16:9] is [15:8] [7:0] is [7:0] |
[17] [8] |
1Kx18 | [17:0] | None |
512x32 (Two-port read) |
A_DOUT[16:9] is [31:24] A_DOUT[7:0] is [23:16] B_DOUT[16:9] is [15:8] B_DOUT[7:0] is [7:0] |
A_DOUT[17] A_DOUT[8] B_DOUT[17] B_DOUT[8] |
512x36 (Two-port read) |
A_DOUT[17:0] is [35:18] B_DOUT[17:0] is [17:0] |
None |
A_BLK AND B_BLK
The following table lists the block port select control signals for the two ports. A_BLK is synchronized by A_CLK while B_BLK is synchronized to B_CLK. Two-port mode is in effect when the width of at least one port is 36, and A_BLK controls the read operation while B_BLK controls the write operation.
Block Port Select Signal | Value | Result |
---|---|---|
A_BLK[2:0] | 111 | Perform read or write operation on Port A. In 36 width mode, perform a read operation from both ports A and B. |
A_BLK[2:0] | Any one bit is 0 | No operation in memory from Port A. Port A read data will be forced to 0. In 36 width mode, the read data from both ports A and B will be forced to 0. |
B_BLK[2:0] | 111 | Perform read or write operation on Port B. In 36 width mode, perform a write operation to both ports A and B. |
B_BLK[2:0] | Any one bit is 0 | No operation in memory from Port B. Port B read data will be forced to 0, unless it is a 36 width mode and write operation to both ports A and B is gated. |
A_WMODE AND B_WMODE
In true dual-port write mode, each port has a feed-through write option:
- Logic 0 = Read data port holds the previous value.
- Logic 1 = Feed-through, that is, write data appears on the corresponding read data port. This setting is invalid when the width of at least one port is 36 and the two-port mode is in effect.
A_CLK AND B_CLK
All signals in ports A and B are synchronous to the corresponding port clock. All address, data, block port select and write enable inputs must be setup before the rising edge of the clock. The read or write operation begins with the rising edge. Two-port mode is in effect when the width of at least one port is 36, and A_CLK provides the read clock while B_CLK provides the write clock:
- A_DOUT_LAT and B_DOUT_LAT
- A_DOUT_CLK and B_DOUT_CLK
- A_DOUT_ARST_N and B_DOUT_ARST_N
- A_DOUT_EN and B_DOUT_EN
- A_DOUT_SRST_N and B_DOUT_SRST_N
The A_DOUT_LAT and B_DOUT_LAT signals select the pipeline registers for the respective port. Two-port mode is in effect when the width of at least one port is 36, and the A_DOUT register signals control the MSB of the read data while the B_DOUT register signals control the LSB of the read data.
The pipeline registers have rising edge clock inputs for each port, which must be tied to the respective port clock when used. When the pipeline registers are not being used, they are forced into latch mode and the clock signals must be tied to 1, which makes them transparent.
The following table lists the functionality of the control signals on the A_DOUT and B_DOUT pipeline registers.
_ARST_N | _LAT | _CLK | _EN | _SRST_N | D | Qn+1 |
---|---|---|---|---|---|---|
0 | X | X | X | X | X | 0 |
1 | 0 | Not rising | X | X | X | Qn |
1 | 0 | — | 0 | X | X | Qn |
1 | 0 | — | 1 | 0 | X | 0 |
1 | 0 | — | 1 | 1 | D | D |
1 | 1 | 0 | X | X | X | Qn |
1 | 1 | 1 | 0 | X | X | Qn |
1 | 1 | 1 | 1 | 0 | X | 0 |
1 | 1 | 1 | 1 | 1 | D | D |
A_EN AND B_EN
These are active-low, and power-down configuration bits for each port. They must be tied to 1.
A_ARST_N AND B_ARST_N
Always tie these signals to 1.
SII_LOCK
Control signal, when 1 locks the entire RAM1K18 memory from being accessed by the SII.
BUSY
This output indicates that the RAM1K18 memory is being accessed by the SII.
RAM64X18
The RAM64x18 block contains 1,152 memory bits and is a three-port memory providing one write port and two read ports. Write operations to the RAM64x18 memory are synchronous. Read operations can be asynchronous or synchronous for either setting up the address and/or reading out the data. Enabling synchronous operation at the read address port improves setup timing for the read address and its enable signals. Enabling synchronous operation at the read data port improves clock-to-out delay. Each data port on the RAM64x18 memory can be independently configured in any combination as shown in the following list:
- 64x18, 64x16
- 128x9, 128x8
- 256x4
- 512x2
- 1Kx1
The main features of the RAM64x18 memory block are as follows:
- There are two independent read data ports A and B, and one write data port C.
- The write operation is always synchronous. The write address, write data, C block port select and write enable inputs are registered.
- For both read data ports, setting up the address can be synchronous or asynchronous.
- The two read data ports have address registers with a separate enable, synchronous-reset, and asynchronous-reset for synchronous mode operation, which can also be configured to be transparent latches for asynchronous mode operation.
- The two read data ports have output registers with a separate
enable, synchronous-reset, and asynchronous-reset for pipeline mode operation, which
can also be configured to be transparent latches for asynchronous mode operation.
Therefore, there are four read operation modes for ports A and B:
- Synchronous read address without pipeline registers (sync-async).
- Synchronous read address with pipeline registers (sync-sync).
- Asynchronous read address without pipeline registers (async-async).
- Asynchronous read address with pipeline registers (async-sync).
- Each data port on the RAM64x18 memory can be independently configured in any of the following combinations: 64x18, 64x16, 128x9, 128x8, 256x4, 512x2, and 1Kx1.
- The widths of each port can be different, but they need to be multiples of one another.
- There is an independent clock for each port. The memory is triggered at the rising edge of the clock.
- Read from both ports A and B at the same location is allowed.
- Read and write on the same location at the same time results in unknown data to be read. There is no collision prevention or detection. However, correct data are expected to be written into the memory.
Pin Name | Pin Direction | Type | Description | Polarity |
---|---|---|---|---|
A_ADDR[9:0] | Input | Dynamic | Port A address | — |
A_BLK[1:0] | Input | Dynamic | Port A block selects | High |
A_WIDTH[2:0] | Input | Static | Port A width/depth mode selection | — |
A_DOUT[17:0] | Output | Dynamic | Port A read data | — |
A_DOUT_ARST_N | Input | Dynamic | Port A pipeline register asynchronous reset | Low |
A_DOUT_CLK | Input | Dynamic | Port A pipeline register clock | Rising |
A_DOUT_EN | Input | Dynamic | Port A pipeline register enable | High |
A_DOUT_LAT | Input | Static | Port A pipeline register select | Low |
A_DOUT_SRST_N | Input | Dynamic | Port A pipeline register synchronous reset | Low |
A_ADDR_CLK | Input | Dynamic | Port A address register clock | Rising |
A_ADDR_EN | Input | Dynamic | Port A address register enable | High |
A_ADDR_LAT | Input | Static | Port A address register select | Low |
A_ADDR_SRST_N | Input | Dynamic | Port A address register synchronous reset | Low |
A_ADDR_ARST_N | Input | Dynamic | Port A address register asynchronous reset | Low |
B_ADDR[9:0] | Input | Dynamic | Port B address | — |
B_BLK[1:0] | Input | Dynamic | Port B block selects | High |
B_WIDTH[2:0] | Input | Static | Port B width/depth mode selection | — |
B_DOUT[17:0] | Output | Dynamic | Port B read data | — |
B_DOUT_ARST_N | Input | Dynamic | Port B pipeline register asynchronous reset | Low |
B_DOUT_CLK | Input | Dynamic | Port B pipeline register clock | Rising |
B_DOUT_EN | Input | Dynamic | Port B pipeline register enable | High |
B_DOUT_LAT | Input | Static | Port B pipeline register select | Low |
B_DOUT_SRST_N | Input | Dynamic | Port B pipeline register synchronous reset | Low |
B_ADDR_CLK | Input | Dynamic | Port B address register clock | Rising |
B_ADDR_EN | Input | Dynamic | Port B address register enable | High |
B_ADDR_LAT | Input | Static | Port B address register select | Low |
B_ADDR_SRST_N | Input | Dynamic | Port B address register synchronous reset | Low |
B_ADDR_ARST_N | Input | Dynamic | Port B address register asynchronous reset | Low |
C_ADDR[9:0] | Input | Dynamic | Port C address | — |
C_CLK | Input | Dynamic | Port C clock | Rising |
C_DIN[17:0] | Input | Dynamic | Port C write data | — |
C_WEN | Input | Dynamic | Port C write enable | High |
C_BLK[1:0] | Input | Dynamic | Port C block selects | High |
C_WIDTH[2:0] | Input | Static | Port C width/depth mode selection | — |
A_EN | Input | Static | Port A power-down (must be tied to 1) | Low |
B_EN | Input | Static | Port B power-down (must be tied to 1) | Low |
C_EN | Input | Static | Port C power-down (must be tied to 1) | Low |
SII_LOCK | Input | Static | Lock access to SII | High |
BUSY | Output | Dynamic | Busy signal from SII | High |
Signal Descriptions for RAM64x18
A_WIDTH, B_WIDTH AND C_WIDTH
The following table lists the width/depth mode selections for each port.
Depth x Width | A_WIDTH/B_WIDTH/C_WIDTH |
---|---|
1Kx1 | 000 |
512x2 | 001 |
256x4 | 010 |
128x8, 128x9 | 011 |
64x16, 64x18 | 1xx |
C_WEN
This is the write enable signal for port C.
A_ADDR, B_ADDR AND C_ADDR
The following table lists the address buses for each port. 10 bits are required to address 1K independent locations in x1 mode. In wider modes, fewer address bits are used. The required bits are MSB justified and unused LSB bits must be tied to 0.
Depth x Width | A_ADDR/B_ADDR/C_ADDR | |
---|---|---|
Used Bits | Unused Bits (must be tied to zero) |
|
1Kx1 | [9:0] | None |
512x2 | [9:1] | [0] |
256x4 | [9:2] | [1:0] |
128x8, 128x9 | [9:3] | [2:0] |
64x16, 64x18 | [9:4] | [3:0] |
C_DIN
The following table lists the write data input for port C. The required bits are LSB justified and unused MSB bits must be tied to 0.
Depth x Width | C_DIN | |
---|---|---|
Used Bits | Unused Bits (must be tied to 0) |
|
1Kx1 | [0] | [17:1] |
512x2 | [1:0] | [17:2] |
256x4 | [3:0] | [17:4] |
128x8 | [7:0] | [17:8] |
128x9 | [8:0] | [17:9] |
64x16 | [16:9] [7:0] |
[17] [8] |
64x18 | [17:0] | None |
A_DOUT AND B_DOUT
The following table lists the read data output buses for ports A and B. The required bits are LSB justified.
Depth x Width | A_DOUT/B_DOUT | |
---|---|---|
Used Bits | Unused Bits | |
1Kx1 | [0] | [17:1] |
512x2 | [1:0] | [17:2] |
256x4 | [3:0] | [17:4] |
128x8 | [7:0] | [17:8] |
128x9 | [8:0] | [17:9] |
64x16 | [16:9] [7:0] | [17] [8] |
64x18 | [17:0] | None |
A_BLK, B_BLK AND C_BLK
The following table lists the block port select control signals for the ports.
Block Port Select Signal | Value | Result |
---|---|---|
A_BLK[1:0] | Any one bit is 0 | Port A is not selected and its read data are forced to zero. |
11 | Perform read operation from port A. | |
B_BLK[1:0] | Any one bit is 0 | Port B is not selected and its read data are forced to zero. |
11 | Perform read operation from port B. | |
C_BLK[1:0] | Any one bit is 0 | Port C is not selected. |
11 | Perform write operation to port C. |
C_CLK
All signals on port C are synchronous to this clock signal. All write address, write data, C block port select and write enable inputs must be setup before the rising edge of the clock. The write operation begins with the rising edge:
- A_DOUT_LAT, A_ADDR_LAT, B_DOUT_LAT, and B_ADDR_LAT
- A_DOUT_CLK, A_ADDR_CLK, B_DOUT_CLK, and B_ADDR_CLK
- A_DOUT_ARST_N, A_ADDR_ARST_N, B_DOUT_ARST_N, and B_ADDR_ARST_N
- A_DOUT_EN, A_ADDR_EN, B_DOUT_EN, and B_ADDR_EN
- A_DOUT_SRST_N, A_ADDR_SRST_N, B_DOUT_SRST_N, and B_ADDR_SRST_N
- The _LAT signals select the registers for the respective port.
The address and pipeline registers have rising edge clock inputs for ports A and B. When both the address and pipeline registers for a port are in use, their clock signals must be tied together. When the registers are not being used, they are forced into latch mode and the clock signals must be tied to 1, which makes them transparent.
The following table lists the functionality of the control signals on the A_ADDR, B_ADDR, A_DOUT, and B_DOUT registers.
_ARST_N | _LAT | _CLK | _EN | _SRST_N | D | Qn+1 |
---|---|---|---|---|---|---|
0 | X | X | X | X | X | 0 |
1 | 0 | Not rising | X | X | X | Qn |
1 | 0 | — | 0 | X | X | Qn |
1 | 0 | — | 1 | 0 | X | 0 |
1 | 0 | — | 1 | 1 | D | D |
1 | 1 | 0 | X | X | X | Qn |
1 | 1 | 1 | 0 | X | X | Qn |
1 | 1 | 1 | 1 | 0 | X | 0 |
1 | 1 | 1 | 1 | 1 | D | D |
A_EN, B_EN AND C_EN
Active-Low, power-down configuration bits for each port. They must be tied to 1.
SII_LOCK
Control signal, when 1 locks the entire RAM64X18 memory from being accessed by the SII.
BUSY
Output indicates that the RAM64X18 memory is being accessed by the SII.