19.3.1 MSVT.param File

msvt.param is an auto-generated file that contains parameters required by MSVT to verify design separation. You can modify the contents of this file according to your requirements.

The following is a Top-Level view of an example design.

Figure 19-3. Top-Level Smart Design Showing Different Design Blocks

The following is an example of a msvt.param file. The contents of the msvt.param file depend on your design.

msvt.param File

//************************************************************************
//                                                                        
//  This is input parameters file for MSVT Check program                  
//                                                                        
//************************************************************************

DEVICE = MPF300TS
DESIGN = SD_Top.msvt
VERIFY_BLOCKS = block4_0 block2_0 block3_0 block1_0 pf_smip_0 // empty list means all blocks in design will be verified
REQUIRED_SEPARATION = 1
MAX_VIOLATIONS_PER_REPORT_SECTION = 1
IRS block4_0 block2_0 = block4_0_Y 
IRS block2_0 block4_0 = 
IRS block4_0 block3_0 = 
IRS block3_0 block4_0 = block3_0_dataOut[31] block3_0_dataOut[30] block3_0_dataOut[29] 
        block3_0_dataOut[28] block3_0_dataOut[27] block3_0_dataOut[26] block3_0_dataOut[25] 
        block3_0_dataOut[24] block3_0_dataOut[23] block3_0_dataOut[22] block3_0_dataOut[21] 
        block3_0_dataOut[20] block3_0_dataOut[19] block3_0_dataOut[18] block3_0_dataOut[17] 
        block3_0_dataOut[16] block3_0_dataOut[15] block3_0_dataOut[14] block3_0_dataOut[13] 
        block3_0_dataOut[12] block3_0_dataOut[11] block3_0_dataOut[10] block3_0_dataOut[9] 
        block3_0_dataOut[8] block3_0_dataOut[7] block3_0_dataOut[6] block3_0_dataOut[5] 
        block3_0_dataOut[4] block3_0_dataOut[3] block3_0_dataOut[2] block3_0_dataOut[1] 
        block3_0_dataOut[0] 
IRS block4_0 block1_0 = block4_0_TX block4_0_Y_0 
IRS block1_0 block4_0 = block1_0_TX 
IRS block4_0 pf_smip_0 = 
IRS pf_smip_0 block4_0 = 
IRS block2_0 block3_0 = 
IRS block3_0 block2_0 = 
IRS block2_0 block1_0 = block1_0_APBmslave0_PRDATA[31] block1_0_APBmslave0_PRDATA[30] 
        block1_0_APBmslave0_PRDATA[29] block1_0_APBmslave0_PRDATA[28] block1_0_APBmslave0_PRDATA[27] 
        block1_0_APBmslave0_PRDATA[26] block1_0_APBmslave0_PRDATA[25] block1_0_APBmslave0_PRDATA[24] 
        block1_0_APBmslave0_PRDATA[23] block1_0_APBmslave0_PRDATA[22] block1_0_APBmslave0_PRDATA[21] 
        block1_0_APBmslave0_PRDATA[20] block1_0_APBmslave0_PRDATA[19] block1_0_APBmslave0_PRDATA[18] 
        block1_0_APBmslave0_PRDATA[17] block1_0_APBmslave0_PRDATA[16] block1_0_APBmslave0_PRDATA[15] 
        block1_0_APBmslave0_PRDATA[14] block1_0_APBmslave0_PRDATA[13] block1_0_APBmslave0_PRDATA[12] 
        block1_0_APBmslave0_PRDATA[11] block1_0_APBmslave0_PRDATA[10] block1_0_APBmslave0_PRDATA[9] 
        block1_0_APBmslave0_PRDATA[8] block1_0_APBmslave0_PRDATA[7] block1_0_APBmslave0_PRDATA[6] 
        block1_0_APBmslave0_PRDATA[5] block1_0_APBmslave0_PRDATA[4] block1_0_APBmslave0_PRDATA[3] 
        block1_0_APBmslave0_PRDATA[2] block1_0_APBmslave0_PRDATA[1] block1_0_APBmslave0_PRDATA[0] 
        block1_0_APBmslave0_PREADY 
IRS block1_0 block2_0 = block1_0_APBmslave0_PADDR[11] block1_0_APBmslave0_PADDR[10] 
        block1_0_APBmslave0_PADDR[9] block1_0_APBmslave0_PADDR[8] block1_0_APBmslave0_PADDR[7] 
        block1_0_APBmslave0_PADDR[6] block1_0_APBmslave0_PADDR[5] block1_0_APBmslave0_PADDR[4] 
        block1_0_APBmslave0_PADDR[3] block1_0_APBmslave0_PADDR[2] block1_0_APBmslave0_PADDR[1] 
        block1_0_APBmslave0_PADDR[0] block1_0_APBmslave0_PWDATA[31] block1_0_APBmslave0_PWDATA[30] 
        block1_0_APBmslave0_PWDATA[29] block1_0_APBmslave0_PWDATA[28] block1_0_APBmslave0_PWDATA[27] 
        block1_0_APBmslave0_PWDATA[26] block1_0_APBmslave0_PWDATA[25] block1_0_APBmslave0_PWDATA[24] 
        block1_0_APBmslave0_PWDATA[23] block1_0_APBmslave0_PWDATA[22] block1_0_APBmslave0_PWDATA[21] 
        block1_0_APBmslave0_PWDATA[20] block1_0_APBmslave0_PWDATA[19] block1_0_APBmslave0_PWDATA[18] 
        block1_0_APBmslave0_PWDATA[17] block1_0_APBmslave0_PWDATA[16] block1_0_APBmslave0_PWDATA[15] 
        block1_0_APBmslave0_PWDATA[14] block1_0_APBmslave0_PWDATA[13] block1_0_APBmslave0_PWDATA[12] 
        block1_0_APBmslave0_PWDATA[11] block1_0_APBmslave0_PWDATA[10] block1_0_APBmslave0_PWDATA[9] 
        block1_0_APBmslave0_PWDATA[8] block1_0_APBmslave0_PWDATA[7] block1_0_APBmslave0_PWDATA[6] 
        block1_0_APBmslave0_PWDATA[5] block1_0_APBmslave0_PWDATA[4] block1_0_APBmslave0_PWDATA[3] 
        block1_0_APBmslave0_PWDATA[2] block1_0_APBmslave0_PWDATA[1] block1_0_APBmslave0_PWDATA[0] 
        block1_0_APBmslave0_PENABLE block1_0_APBmslave0_PSELx block1_0_APBmslave0_PWRITE 
IRS block2_0 pf_smip_0 = 
IRS pf_smip_0 block2_0 = 
IRS block3_0 block1_0 = block3_0_dataOut_0[7] block3_0_dataOut_0[6] block3_0_dataOut_0[5] 
        block3_0_dataOut_0[4] block3_0_dataOut_0[3] block3_0_dataOut_0[2] block3_0_dataOut_0[1] 
        block3_0_dataOut_0[0] 
IRS block1_0 block3_0 = block1_0_dataOut[7] block1_0_dataOut[6] block1_0_dataOut[5] 
        block1_0_dataOut[4] block1_0_dataOut[3] block1_0_dataOut[2] block1_0_dataOut[1] 
        block1_0_dataOut[0] 
IRS block3_0 pf_smip_0 = 
IRS pf_smip_0 block3_0 = 
IRS block1_0 pf_smip_0 = 
IRS pf_smip_0 block1_0 = 
REGIONS_VERBOSITY = 0

Table 19-1. Parameters in the msvt.param File
ParameterDescription
DEVICEName of the Microchip FPGA device implementing the design.
DESIGNLocation of the files required for MSVT. By default, it will point to the auto-generated msvt.dtf folder.
VERIFY BLOCKSContains a list of blocks to be verified. By default, all the block names present in the design are listed. You can modify this list and include a subset of blocks to be audited by MSVT.
REQUIRED_SEPARATIONRequired separation parameter per the guideline requirements. The default value is 1.
MAX_VIOLATIONS_PER_REPORT_SECTIONControls the number of violations that are to be reported in each section. The default value is 1.
IRSContains a list of IRS signal names present in the design. Each IRS statement is comprised of a pair of separated blocks followed by a list of the IRS signal names between them.
REGIONS_VERBOSITYControls reporting of each routing region and the assigned instances. The default value is 0.

You can modify the parameters in the msvt.param file to refine your verification criteria. We recommend modifying the REQUIRED_SEPARATION parameter according to your system requirements before executing MSVT. You can also specify the blocks you want to verify, the names of each IRS signal, and add a limit to the max number of violations to be reported.