15.1.13 FlashPro Express Reference

Use this chapter as a reference for the FlashPro Express user interface.

15.1.13.1 FlashPro Express Start Page

The FlashPro Express Start page is the first page that appears when the tool starts. This page provides the interface for loading a project into the tool by either navigating to the project location or clicking a recently opened project.

15.1.13.2 FlashPro Express Project Menu

The following table lists the FlashPro express project menu details.

Table 15-17. FlashPro Express Project Menu
CommandFunction

New Job Project

New job project folder with programming job name will be created at the specified location.

Open Job Project

Loads a job project into the tool by reading the information in the user-specified .pro file.

Close Job Project

Closes the current job project.

Save Job Project

Saves the current job project.

Set Log File

Sets the location of the Log file to your specified location.

Export Log File

Exports the Log file to your specified location.

Preferences

Allows you to select FlashPro Express mode.

Execute Script

Runs your specified Tcl script.

Export Script File

Exports all commands run in this session to your specified path as a Tcl script.

Exit

Exits FlashPro Express.

15.1.13.3 FlashPro Express Edit Menu

Table 15-18. FlashPro Express Edit Menu
Command Function

Clear Log Window

Clears the Log window.

15.1.13.4 FlashPro Express View Menu

Table 15-19. FlashPro Express View Menu
Command Function

Log Window

Shows or hides the Log window.

15.1.13.5 FlashPro Express Tools Menu

The following table lists the FlashPro express tools menu details.

Table 15-20. FlashPro Express Tools Menu
CommandFunction
Programming Connectivity and InterfaceThe Programming Connectivity and Interface window displays the physical chain from TDI to TDO or SPI Target configuration.

Programmer Settings

Opens the Programmer Settings dialog box in which you can set options for supported Microchip programmers.

Disable Core Check During Scan and Check Chain

Disables core checking during scan and check chain operations.

15.1.13.6 FlashPro Express Help Menu

Table 15-21. FlashPro Express Help Menu
Command Function

Help Topics

Opens the help.

Microchip Technical Support

Opens the Microchip technical support site.

Microchip Web Site

Opens the Microchip Website in your default browser.

User Guide

Opens the FlashPro Express User Guide.

Check for Software Updates

Checks for software updates if you are connected to the Internet.

About FlashPro Express

Lists the FlashPro Express release information.

15.1.13.7 FlashPro Express Log Window and Status Bar

The following sections describe the FlashPro Express Log window and status bar.

15.1.13.7.1 FlashPro Express Log Window

The FlashPro Express Log window shows status messages for user activity.

  • Click the appropriate tab (Messages, Errors, Warning, and Info) to filter messages by type.
  • Use the right-click menu to copy text, clear the log, and scroll the log.
  • Use the def variable LOG_WINDOW_BUFFER_SIZE to set the buffer size.
  • Use the View menu to show or hide the Log window.

15.1.13.7.2 FlashPro Express Status Bar

The Status Bar at the bottom shows the status of the load project action.