9.2.1 Port Name

This is the port list of the design. The ports of the design are displayed in a structured manner according to group name/functions. Ports can be expanded or collapsed. The port list can be sorted or filtered, in a way similar to the Windows spreadsheet operations. For example, entering RESET in the match field in the filter returns a list of port names that have RESET in the port name.