9.2.18 ODT Dynamic
(Ask a Question)Note: This option is supported for RTG4 production devices only.
This option is used to opt in or out of the dynamic ODT set on a bank. Possible value are listed in the following table.
Value | Description |
---|---|
ODT_STATIC=On ODT_DYNAMIC=On | Illegal |
ODT_STATIC=On ODT_DYNAMIC=Off | The ODT resistor is always turned on. |
ODT_STATIC=Off ODT_DYNAMIC=Off | The ODT resistor is always turned off. |
ODT_STATIC=Off ODT_DYNAMIC=On | The ODT resistor is on or off based on the ODT Dynamic bank setting. |
The following I/O standards are supported:
- LVDS
- RSDS
- MINILVDS
- LVPECL
- HSTLI
- HSTLII
- SSTL15I
- SSTL15II
- SSTL18I
- SSTL18II
- HSTL18I
- HSTL18II
- LPDDRI
- LPDDRII
Note: There is a known issue in the Libero SoC I/O
Editor and the pin report. A software limitation exists where a design cannot have
different values for the P and N sides. Currently, both must have the same value. Libero
SoC does program the P and N side correctly for programming. In I/O Editor or pin
report, if RES_PULL is Up on both, it means the N side is programmed as Down or vice
versa.