3.6.1 SmartHLS Pragmas Manual
(Ask a Question)Learn more about the pragmas available for SmartHLS.
3.6.1.1 Introduction to Pragmas
(Ask a Question)SmartHLS™ accepts pragma directives in the source code to guide the hardware generation. This reference section explains all of the pragmas available for SmartHLS.
#pragma HLS <category> <feature> <parameter>(<value>)
function: configure a hardware function.loop: configure loop optimizations.interface: configure hardware interfaces (arguments / global variables).memory: configure hardware memory implementation.
Each category can have different configurable features. Some categories / features have parameters to passed to the pragma. A parameter can be optional with a default behaviour if not specified. The value of a parameter can be either integer, boolean (true|false), name (variable / argument), or a set of pre-specified values.
Note
For integer parameters, the user is allowed to use constants (or expressions of constants) defined using #define directive. For example, this is allowed:
#define N 10 void fun() { #pragma HLS loop unroll factor(N+1) for (int i = 0; i < 100; i++) ... }
- At the beginning of function definition block before any other statements.
 - Before global / local variable declaration.
 - Before loop block.
 
3.6.1.2 Pipeline Loop
(Ask a Question)- Syntax
 #pragma HLS loop pipeline II(<int>)- Description
 - This pragma enables pipelining for a given loop in the code. Loop pipelining allows a new iteration of the loop to begin before the current one has completed, achieving higher throughput. It can be specified to pipeline a single loop or a nested loop. If specified on a single loop or on a inner loop of a nested loop, that loop will be pipelined. If specified on the outer loop of a nested loop, the outer loop will be pipelined and all of its inner loops will be automatically unrolled.
 - Parameters
 Parameter Value Optional Default Description IIInteger Yes 1 Pipeline initiation interval - Position
 - Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
 - Examples
 #pragma HLS loop pipeline II(2) for (int i = 0; i < 10; i++) { ... }
LOOP_LABEL: #pragma HLS loop pipeline while (i < 10) { ... }
3.6.1.3 Unroll Loop
(Ask a Question)- Syntax
 #pragma HLS loop unroll factor(<int>)- Description
 - Specifies a loop to be unrolled. The factor indicates how many times to unroll the loop. If it is not specified, or specified as N (the total number of loop iterations), the loop will be fully unrolled. If it is specified as 2, the loop will be unrolled 2 times, where the number of loop iterations will be halved and the loop body will be replicated twice. If it is specified as 1, the loop will NOT be unrolled.
 - Parameters
 Parameter Value Optional Default Description factorInteger Yes N (fully unroll) Unroll count - Position
 - Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
 - Examples
 #pragma HLS loop unroll factor(1) for (int i = 0; i < 10; i++) { ... }
3.6.1.4 Bound Loop
(Ask a Question)- Syntax
 #pragma HLS loop bounds lower(<int>) upper(<int>)- Description
 - Specifies the bounds on the number of times a loop will iterate. This pragma does not affect the synthesized circuit. It's only used to improve reporting. By manually specifying bounds, the overall loop latency can be computed and reported.
 - Parameters
 - 
                    
Parameter Value Optional Default Description lowerInteger No - Lower bound upperInteger No - Upper bound  - Position
 - Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
 - Examples
 - 
                    
#pragma HLS loop bounds lower(5) upper(10) // Here, the bounds tell us the trip count (number of iterations) will be between 5 and 10 inclusively. for (int i = 0; i < N; i++) { ... }
 
3.6.1.5 Loop Dependence
(Ask a Question)- Syntax
 #pragma HLS loop dependence variable(<var_name>) type(inter) direction(RAW|WAR|WAW) dependent(true|false)- Description
 - Specifies the loop-carried dependence of a variable to eliminate false
                    dependency and improve pipeline initiation interval (II). 
HLS loop dependencepragma configuration overrides the loop dependency analysis result in the tool.Important: Users are advised to carefully verify the loop dependency information specified. An incorrect loop dependency information leads the tool to generate incorrect hardware design. - Parameters
 - 
                    
Parameter Value Optional Default Description variable/argumentString No - Variable/Argument Name. typeinterNo - Dependence Type. interis the dependence between different loop iterations.directionRAW|WAR|WAWYes - Specifies the loop dependence direction. Only valid for Whentype(inter).directionis not specified, thedependentparameter is applicable to all 3 directions.dependenttrue|falseYes falseSpecifies if there is a loop-carried dependence for the given typeanddirection. - Position
 - Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
 - Examples
 - 
                    
int f(int x[100], int j /*j is odd*/) { int res = 0; loop: #pragma HLS loop pipeline #pragma HLS loop dependence argument(x) type(inter) direction(RAW) dependent(false) for (int i = 0; i < 100; i = i + 2 /*i is even*/) { res += x[i]; x[i + j] += 1; } return res; }
 
3.6.1.6 Inline Function
(Ask a Question)- Syntax
 #pragma HLS function inline- Description
 - This pragma forces a given function to be inlined.
 - Position
 - At the beginning of the function definition block.
 - Examples
 - 
                    
int sum(int *a) { #pragma HLS function inline ... } 
3.6.1.7 Noinline Function
(Ask a Question)- Syntax
 #pragma HLS function noinline- Description
 - This pragma prevents a given function from being inlined.
 - Position
 - At the beginning of the function definition block.
 - Examples
 - 
                    
int sum(int *a) { #pragma HLS function noinline ... } 
3.6.1.8 Replicate Function
(Ask a Question)- Syntax
 #pragma HLS function replicate- Description
 - This pragma specifies a function to be replicated every time it is called. By default, when the circuit is not pipelined, SmartHLS™ creates a single instance for each function which is shared across multiple calls to the function. When using this pragma on the function, SmartHLS will create a new instance of the function for every function call.
 - Position
 - At the beginning of the function definition block.
 - Examples
 int sum(int *a) { #pragma HLS function replicate ... }
3.6.1.9 Flatten Function
(Ask a Question)- Syntax
 #pragma HLS function flatten branchless(true|false)- Description
 - This pragma unrolls all loops and inlines all subfunctions for a given function. If the 
branchlessoption is set to true, all branches (e.g., if-else, switch) in the specified function will also be flattened to allow more parallelism between operations, specifically between the operations that are under different-yet-independent conditions. - Parameters
 Parameter Value Optional Default Description branchlesstrue|false Yes truetrueto flatten branch statements- Position
 - At the beginning of the function definition block.
 - Examples
 int sum(int *a) { #pragma HLS function flatten branchless(true) ... }
3.6.1.10 Set Top-Level Function
(Ask a Question)- Syntax
 #pragma HLS function top- Description
 - This pragma specifies the top-level C/C++ function. The top-level function and all of its descendant functions will be compiled to hardware.
 - Position
 - At the beginning of the function definition block.
 - Examples
 - 
                    
int sum(int *a) { #pragma HLS function top ... } 
3.6.1.11 Pipeline Function
(Ask a Question)- Syntax
 #pragma HLS function pipeline II(<int>)- Description
 - This pragma enables pipelining for a given function in the code. Function pipelining allows a new invocation of a function to begin before the current one has completed, achieving higher throughput.
 - Parameters
 Parameter Value Optional Default Description IIInteger Yes 1 Pipeline initiation interval - Position
 - At the beginning of the function definition block.
 - Examples
 int sum(int *a) { #pragma HLS function pipeline ... }int conv(int a[], int b[]) { #pragma HLS function pipeline II(3) ... }
3.6.1.12 Dataflow
(Ask a Question)- Syntax
 #pragma HLS function dataflow- Description
 - Specifies that a function should execute using dataflow parallelism.
 - Position
 - At the beginning of the function definition block.
 - Examples
 - 
                    
void canny(hls::FIFO<unsigned char> &input_fifo, hls::FIFO<unsigned char> &output_fifo) { #pragma HLS function dataflow #pragma HLS dataflow_channel variable(output_gf) type(fifo) unsigned char output_gf [HEIGHT * WIDTH]; #pragma HLS dataflow_channel variable(output_sf) type(fifo) unsigned short output_sf [HEIGHT * WIDTH]; #pragma HLS dataflow_channel variable(output_nm) type(fifo) unsigned char output_nm [HEIGHT * WIDTH]; gaussian_filter(input_fifo, output_gf); sobel_filter(output_gf, output_sf); nonmaximum_suppression(output_sf, output_nm); hysteresis_filter(output_nm, output_fifo); }
 
3.6.1.13 Dataflow Channel
(Ask a Question)- Syntax
 #pragma HLS dataflow_channel variable(<var_name>) type(fifo|shared_buffer|double_buffer) depth(<int>)- Description
 - Specifies that a variable in a dataflow function should be converted to use a particular channel type.
 - Parameters
 Parameter Value Optional Default Description variablestring No - Variable Name typefifo|shared_buffer|double_bufferNo double_bufferChannel type depthInteger Yes 2 FIFO depth (only when type is FIFO) - Position
 - Before the variable declaration.
 - Examples
 - FIFO channels are used for a Canny edge detector, since the pixels are processed in sequential order.
void canny(hls::FIFO<unsigned char> &input_fifo, hls::FIFO<unsigned char> &output_fifo) { #pragma HLS function dataflow #pragma HLS dataflow_channel variable(output_gf) type(fifo) unsigned char output_gf [HEIGHT * WIDTH]; #pragma HLS dataflow_channel variable(output_sf) type(fifo) unsigned short output_sf [HEIGHT * WIDTH]; #pragma HLS dataflow_channel variable(output_nm) type(fifo) unsigned char output_nm [HEIGHT * WIDTH]; gaussian_filter(input_fifo, output_gf); sobel_filter(output_gf, output_sf); nonmaximum_suppression(output_sf, output_nm); hysteresis_filter(output_nm, output_fifo); }
 
3.6.1.14 Scalar Argument Interface
(Ask a Question)- Syntax
 #pragma HLS interface argument(<arg_name>) type(<simple|axi_target>) stable(<false|true>)- Description
 - This pragma configures the RTL interface for a scalar argument. This pragma is ignored if the enclosing function is not specified as the top-level.
 - Parameters
 Parameter Value Optional Default Description argumentstring No Argument name typesimple|axi_targetNo simpleInterface type stabletrue|falseYes falseOnly available for simpletype;trueif the argument is stable.- Position
 - At the beginning of the function definition block.
 - Examples
 int fun(int a) { #pragma HLS function top #pragma HLS interface argument(a) type(simple) stable(true) ... }
3.6.1.15 Memory Interface for Pointer Argument/Global Variable
(Ask a Question)- Syntax
 #pragma HLS interface argument(<arg_name>) type(memory) num_elements(<int>)#pragma HLS interface variable(<var_name>) type(memory) num_elements(<int>)- Description
 - This pragma specifies the memory interface type for a pointer (including array, struct, class types) argument or shared global variable. For more details, see the Memory Interface section. This pragma is ignored if the enclosing function is not specified as the top-level.
 - Parameters
 Parameter Value Optional Default Description argument/variablestring No - Argument/Variable name typememoryNo - Interface type num_elementsinteger Yes - Specifies the number of elements of the argument array. Can override the array size in the argument. - Position
 Argument - At the beginning of the function definition block.
Variable - Before the global variable declaration.
- Examples
 #pragma HLS interface variable(c) type(memory) num_elements(100) int c[100]; int fun(int a[], int b[]) { #pragma HLS function top #pragma HLS interface argument(a) type(memory) num_elements(100) #pragma HLS interface argument(b) type(memory) ... }
3.6.1.16 AXI4 Target Interface for Pointer Argument
(Ask a Question)- Syntax
 #pragma HLS interface argument(<arg_name>) type(axi_target) num_elements(<int>) dma(true|false) requires_copy_in(true|false)- Description
 - This pragma specifies the AXI4 target interface type for a pointer (including array, struct, class types) argument. For more details, see the AXI4 Target Interface section. This pragma is ignored if the enclosing function is not specified as the top-level.
 - Parameters
 Parameter Value Optional Default Description argumentstring No - Argument name typeaxi_targetNo - Interface type num_elementsinteger Yes - Specifies the number of elements of the argument array. Can override the array size in the argument. dma, requires_copy_intrue|falseYes falseSpecifies the transfer method and copy-in behaviour in the top-level driver function. See Top-level Driver Options in Pointer Arguments' AXI4 Target Interface Pragma ecctrue|falseYes falseSpecifies if Error Correction Code is enabled. Set to truefor enabling ECC for AXI4 Target Interface. See Error Correction Code for more information about Error Correction Code.- Position
 - At the beginning of the function definition block.
 - Examples
 int fun(int a[], int b[101]) { #pragma HLS function top #pragma HLS interface argument(a) type(axi_target) num_elements(100) dma(true) requires_copy_in(false) #pragma HLS interface argument(b) type(axi_target) ... }
3.6.1.17 AXI4 Initiator Interface for Pointer Argument
(Ask a Question)- Syntax
 #pragma HLS interface argument(<arg_name>) type(axi_initiator) ptr_addr_interface(<simple|axi_target>) num_elements(<int>) max_burst_len(<int>) max_outstanding_reads(<int>) max_outstanding_writes(<int>)- Description
 - This pragma specifies the AXI4 initiator interface type for a pointer (including array, struct, class types) argument. For more details, see the AXI4 Initiator Interface section. This pragma is ignored if the enclosing function is not specified as the top-level.
 - Parameters
 Parameter Value Optional Default Description argumentstring No - Argument name typeaxi_targetNo - Interface type num_elementsinteger Yes - Specifies the number of elements of the argument array. Can override the array size in the argument. Only needed by the Simulate HLS Hardware (SW/HW Co-Simulation) feature and does not affect HLS-generated RTL. ptr_addr_interfacesimple|axi_targetYes - Specifies the interface type for setting the base address of the accessing memory. The default type is simplebut is changed toaxi_targetif Default All Interfaces to Use AXI4 Target is set.max_burst_leninteger Yes 16 Specifies the maximum burst length for each AXI initiator transaction. Transfers that are larger than the maximum burst length will be split into multiple AXI transactions. The permitted values are between 1 and 256. max_outstanding_readsinteger Yes 1 Specifies the maximum amount of read burst requests to external AXI4 Targets that can be left outstanding (waiting for response) before the accelerator stalls. This infers a FIFO of size max_outstanding_reads*addr_sizefor the AR channel, and a FIFO of sizemax_outstanding_reads*max_burst_len*word_sizefor the R channel. The permitted values are between 1 and 8.max_outstanding_writesinteger Yes 1 Specifies the maximum amount of write burst requests to external AXI4 Targets that can be left outstanding (waiting for response) before the accelerator stalls. This infers a FIFO of size max_outstanding_writes*addr_sizefor the AW channel, and a FIFO of sizemax_outstanding_writes*max_burst_len*word_sizefor the W channel. The permitted values are between 1 and 8.add_4k_boundary_protectionbool Yes true Specifies whether or not SmartHLS™ should generate additional logic to protect AXI4 initiator burst transactions from crossing 4K boundaries for this argument. Setting this field to falsewill remove this alignment logic, but the user must then make sure that any pointer addresses given to the SmartHLS module will not result in bursting accross a 4K address boundary (a violation of the AXI4 spec.- Position
 - At the beginning of the function definition block.
 - Examples
 int fun(int a[]) { #pragma HLS function top #pragma HLS interface argument(a) type(axi_initiator) num_elements(100) ptr_addr_interface(axi_target) max_burst_len(8) #pragma HLS interface argument(a) type(axi_initiator) num_elements(100) max_outstanding_reads(4) max_outstanding_writes(4) ... }
3.6.1.18 Legacy AXI4 Slave Interface for Global Variable
(Ask a Question)- Syntax
 #pragma HLS interface variable(<var_name>) type(axi_slave) concurrent_access(true|false)- Description
 - This pragma specifies the legacy AXI4 slave interface for a global struct. When the 
concurrent_accessoption is set to true (default to false), the external logic can read/write the AXI4 slave interface while the SmartHLS module is running. The concurrent access will however reduce the SmartHLS module's throughput to access the memory. For more details. see the Legacy AXI4 Slave Interface section. This pragma is ignored if the enclosing function is not specified as the top-level. - Parameters
 Parameter Value Optional Default Description variablestring No - Variable name typeaxi_slaveNo - Interface type concurent_accesstrue|falseYes falseEnable/disable concurrent access - Position
 - Before the global variable declaration.
 - Examples
 #pragma HLS interface variable(b) type(axi_slave) concurrent_access(true) int b[SIZE]
3.6.1.19 Module Control Interface
(Ask a Question)- Syntax
 #pragma HLS interface control type(<simple|axi_target>)- Description
 - This pragma configures the Module Control Interface. This pragma is ignored if the enclosing function is not specified as the top-level.
 - Parameters
 - 
                    
Table 3-18. Parameter Value Optional Default Description typesimple|axi_target No simpleInterface type  - Position
 - At the beginning of the function definition block.
 - Examples
 - 
                    
int fun() { #pragma HLS function top #pragma HLS interface control type(simple) ... }
 
3.6.1.20 Default All Interfaces to Use AXI4 Target
(Ask a Question)- Syntax
 #pragma HLS interface default type(axi_target)- Description
 - This pragma specifies the default interface to AXI4 target for all arguments and Module Control Interface. This pragma is ignored if the enclosing function is not specified as the top-level.
 - Parameters
 Parameter Value Optional Default Description typeaxi_target No - Interface type - Position
 - At the beginning of the function definition block.
 - Examples
 // The following two functions have the same interface configurations. // Without using default interface pragma: int fun(int a, int b[10], int c[20], int d[30]) { #pragma HLS function top #pragma HLS interface control type(axi_target) #pragma HLS interface argument(a) type(axi_target) #pragma HLS interface argument(b) type(axi_target) #pragma HLS interface argument(c) type(axi_target) dma(true) #pragma HLS interface argument(d) type(axi_initiator) ptr_addr_interface(axi_target) ... } // Use default interface pragma: int fun(int a, int b[10], int c[20], int d[30]) { #pragma HLS function top #pragma HLS interface default type(axi_target) #pragma HLS interface argument(c) type(axi_target) dma(true) // Note that 'ptr_addr_interface(axi_target)' can be omitted when default interface is set to axi_target. #pragma HLS interface argument(d) type(axi_initiator) ... }
3.6.1.21 Contention-Free Memory Access
(Ask a Question)- Syntax
 #pragma HLS memory impl variable(<arg_name>) contention_free(true|false)- Description
 - The pragma is to be used for variables accessed by parallel functions (
hls::thread) so that SmartHLS™ does not create arbiters for the specified variable. The specified variable can still be accessed by multiple concurrently running functions, but without contention. It will be the users' responsibility to ensure at most one function may access the shared variable in a clock cycle. If not specified, by default, SmartHLS creates arbiters for variables that are accessed by parallel functions. - Parameters
 Parameter Value Optional Default Description variablestring No - Variable Name contention_freetrue|falseYes falsetruefor contention-free access- Position
 - Before the global / local variable declaration.
 - Examples
 #pragma HLS memory impl variable(b) contention_free(true) int b[100]
3.6.1.22 Struct Variable/Argument Packing
(Ask a Question)- Syntax
 #pragma HLS memory impl variable(<var_name>) pack(bit|byte) byte_enable(true|false)#pragma HLS memory impl argument(<arg_name>) pack(bit|byte) byte_enable(true|false- Description
 - The pragma is to be used to pack a global interface / local memory variable with 
structtype. There are two packing modes:bit/bytewherebitpacking packs thestructfields using the exact bit-width andbytemode packs the fields with 8-bit alignment.byte_enableoption creates an interface / memory with byte enable signals to write individual fields when set totrue. Note thatbyte_enableis only valid withbytepacking. - Parameters
 Parameter Value Optional Default Description variable/argumentstring No - Variable/Argument Name packbit|byteNo - Packing Mode byte_enabletrue|falseYes falseUse byte-enable to write stuct fields - Position
 Argument - At the beginning of the function definition block.
Variable - Before the global / local variable declaration.
- Examples
 #pragma HLS memory impl variable(b) pack(bit) struct S b[100]; int sum(struct S &s) { #pragma HLS function top #pragma HLS memory impl argument(s) pack(byte) byte_enable(true) ... }
3.6.1.23 Partition Memory
(Ask a Question)- Syntax
 #pragma HLS memory partition variable(<var_name>) type(block|cyclic|complete|struct_fields|none) dim(<int>) factor(<int>)- Description
 - This pragma specifies a variable to be partitioned. Dimension 1 corresponds to the left-most dimension of an array and higher dimensions correspond to right-ward dimensions. The 
dimparameter is only applicable forblock|cyclic|completetypes. Ifdimis 0, the specified partitioning will be applied to all dimensions. Thefactorparameter is only applicable forblock|cyclictypes to specify the number of partitions.factormust be larger than 1. For more details about the pragma options, see User-Specified Memory Partitioning. - Parameters
 Parameter Value Optional Default Description variablestring No - Variable name typeblock, cyclic, complete, struct_fields, noneYes completePartition type diminteger Yes 0 Partition dimension factorinteger Yes - Number of partitions - Position
 - Before the global / local variable declaration.
 - Examples
 #pragma HLS memory partition variable(b) type(none) int b[100]; int fun(int *a) { ... #pragma HLS memory partition variable(c) type(block) dim(1) factor(2) int c[100][100]; ... }
3.6.1.24 Partition Top-Level Interface
(Ask a Question)- Syntax
 #pragma HLS memory partition argument(<arg_name>) type(block|cyclic|complete|struct_fields|none) dim(<int>) factor(<int>)- Description
 - This pragma specifies a top-level argument to be partitioned. Dimension 1 corresponds to the left-most dimension of an array and higher dimensions correspond to right-ward dimensions. The 
dimparameter is only applicable forblock|cyclic|completetypes. Ifdimis 0, the specified partitioning will be applied to all dimensions. Thefactorparameter is only applicable forblock|cyclictypes to specify the number of partitions.factormust be larger than 1. For more details about the pragma options, see .User-Specified Memory Partitioning - Parameters
 Parameter Value Optional Default Description argumentstring No - Argument name typeblock, cyclic, complete, struct_fields, noneYes completePartition type diminteger Yes 0 Partition dimension factorinteger Yes - Number of partitions - Position
 - At the beginning of the function definition block.
 - Examples
 int sum(int *a, int *b) { #pragma HLS function top #pragma HLS memory partition argument(a) type(cyclic) dim(2) factor(4) #pragma HLS memory partition argument(b) }
3.6.1.25 Replicate ROM
(Ask a Question)- Syntax
 #pragma HLS memory replicate_rom variable(<rom_var_name>) max_replicas(<int>)- Description
 - This pragma can be used to replicate constant memory (i.e., arrays) to achieve better throughput (shorter cycle latency) at the expense of extra resource (e.g., block RAM). Typically when an array is implemented in block RAMs, there are up-to-two RAM ports to allow a maximum of two reads per clock cycle. To allow more parallel read accesses in each clock cycle, constant read-only memories (ROM) can be replicated by using this pragma.
 - Parameters
 Parameter Value Optional Default Description max_replicasinteger Yes 0 The maximum number of replicas allowed - Position
 - Before the global / local variable declaration.
 - Examples
 #pragma HLS memory replicate_rom variable(my_rom) max_replicas(10) const int my_rom[100]
3.6.1.26 Error Correction Code
(Ask a Question)- Syntax
 #pragma HLS memory impl variable(<var_name>) ecc(true|false)- Description
 - This pragma enables generating Error Correction Code (ECC) protected memory.
 - Parameters
 Parameter Value Optional Default Description variablestring No Variable name ecctrue|falseyes falsetruefor enabling ECC- Position
 - Before the global / local variable declaration.
 - Examples
 #pragma HLS memory impl variable(x) ecc(true) int x[100];