6.4.2 Managing Place and Route and Globals
(Ask a Question)The Place-and-Route tool has an option to limit the number of row globals used for block creation.
To use this option:
- From the Design Flow window, right-click Place and Route and choose Configure Options.The Layout Options dialog box shows the default number of row-global resources for the technology family.
 - Enter a value to restrict the number of row-global resources available in every half-row of the device. During Place and Route of the block, the tool will not exceed this capacity on any half-row. The default value is the maximum number of row globals. If you enter a value lower than the maximum capacity (the default), the layout of the block will be able to integrate with the rest of the design if the remaining row-global capacity is consumed.