9.6.4 Making I/O Assignments
(Ask a Question)To make I/O assignment for the Memory Interface instance in the design:
- Select the Memory Interface type from the drop-down menu.
 - From the Ports tab in the Design Tree View, drag the Memory Interface instance and let the mouse hover over one of the Edge_Anchor locations available for the Memory Interface type. A tooltip reports whether it is a legal or illegal location for the Interface instance.
 - Drop the Interface instance into a legal Edge_Anchor location.
 - 
            Check that no DRC error messages are reported in the Log window
               and the I/O assignments are accepted (see the following figure). The Lock icon in the
               Ports tab indicates that the I/O assignment is accepted and locked.
            
Figure 9-9. Memory Interface Assignments Accepted 
 
Note: DRC rules are enforced. Drag-and-drop I/O placement that violates the DRC rules
                  are reported in the Log window. For Memory Interface, the DRC checks the Data
                  Width and the Data Rate compliance*. If the specific location cannot accommodate
                  the Data Width or the Data Rate of the Memory interface, no I/O assignment is
                  made. An error is reported in the Log Window with a message that explains why the
                  assignment is not accepted. In the following figure, the DRC error message reports
                  that the ddr3 instance requires 64 ports, but the SOUTH_SE location can
                  accommodate only 58 pins.
            Note: *Data Rate compliance will be enforced in a later release.