9.6.5 IO_PDC File
(Ask a Question)When the I/O assignment is committed and saved in the I/O Editor, the assignment is saved in a PDC file in the <project_folder/constraints/io/user.pdc> file. The PDC file contains set_io commands on each of the DDR Memory Interface I/O.
The following figure shows PDC file generation after Memory interface I/O assignment in the I/O Editor.