8.2 Push
(Ask a Question)To go down one level of hierarchy in the Netlist Viewer:
- Click to select the instance.
- Click the Push icon on the Toolbar or right click and select Push Instance <Instance_name> or double click a pushable instance (not at the bottom of the design hierarchy) to push into the instance.
Important: The right-mouse click push instance menu item is not available at the bottom of the
design hierarchy.
You can also select one pin of an instance, and then choose Push from the right click menu to move the focus to that pin. For example, if you select pin N_972 of UCORE and choose Push from the right click menu as shown in the following figure, Netlist Viewer centers on the port corresponding to the pin you selected as shown.