21.16.5 remove_hsm_tickets
(Ask a Question)Description
This Tcl
                command removes HSM tickets from the HSM using one of the following methods: 
- By specifying the job reply file in which case all tickets that are in the reply file is deleted.
 - By specifying each of the ticket IDs value in hexadecimal string.
 
Important: 
- This command must be used very carefully as it removes HSM tickets, rendering any FlashPro Express jobs based on those tickets to be unusable.
 - This command does not require a FlashPro Express project to be created or opened.
 
remove_hsm_tickets [-ticket_ids "Ticket IDs to remove"] \
                   [-reply_file "Reply file containing ticket IDs to remove"] \
		   [-force "TRUE | FALSE"]Arguments
| Parameter | Type | Description | 
|---|---|---|
| ticket_ids | hexadecimal | Specifies Hex value of each ticket ID to be removed. This parameter is optional. This parameter can specify several values separated by spaces. | 
| reply_file | string | Specifies full file name of job request file. This parameter is optional. | 
| force | boolean | This parameter is optional. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Specify one of the required arguments: 'ticket_ids' or 'reply_file'. | 
| None | 'value' is not a valid hex string. Specify a valid hex string for ticket ID. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is remove_hsm_tickets [-ticket_ids "[Ticket IDs to remove]+"] \ [-reply_file "Reply file containing ticket IDs to remove"] \ [-force "TRUE | FALSE"]'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
This example removes the HSM tickets from the HSM by specifying Job reply file:
remove_hsm_tickets \
		    -reply_file {D:flashpro_filesjobmgr_project12cm_reply.rep}This example removes the HSM tickets from the HSM by specifying each of the ticket IDs value in hexadecimal string.
remove_hsm_tickets \
         -ticket_ids {00000000000000000000899f252d9fb55442aa7e 00000000000000000000b6f385c6a9eeca69705c 00000000000000000000ed5702d0b767ba686b82}