Description
This Tcl
                command processes a job request received from Job Manager. It is part of the Job
                Ticket generation process.
Important: HSM server name must be specified via HSM_SERVER_NAME DEF
            variable.
process_job_request -request_file "job request file" \
                    -reply_file "job reply file" \
		    [-overwrite_reply "TRUE | FALSE"]
Arguments
| Parameter | Type | Description | 
|---|
| request_file | string | Specifies full file name of job request file. This parameter is
                                mandatory. | 
| reply_file | string | Specifies full file name of job reply file. This parameter is
                                mandatory. | 
| overwrite_reply | boolean | This parameter is optional. The possible value of this parameter
                                are the following: - TRUE or 1:
                                        Allows overwriting of any pre-existing reply_file.
 - FALSE or 0:
                                        Does not allow overwriting of any pre-existing
                                        reply_file.
 
  | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'request_file' is missing. | 
| None | Required parameter 'reply_file' is missing. | 
| None | Parameter 'request_file' : the file '/request_file_name' does not
                                exist. | 
| None | overwrite_reply: Invalid argument value: 'value' (expecting TRUE,
                                1, true, FALSE, 0 or false). | 
| None | Cannot get HSM. | 
| None | Parameter 'param_name' is not defined. Valid command formatting
                                is 'process_job_request -request_file "job request file" \
                                -reply_file "job reply file" \ [-overwrite_reply "TRUE |
                                FALSE"]'. | 
Supported Families
| PolarFire® | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
| PolarFire SoC | 
Example
This example
                processes a job
            request:
process_job_request \
        -request_file {D:/flashpro_files/jobmgr_project/cm_request.req} \
        -reply_file {D:/flashpro_files/jobmgr_project/cm_reply.rep} \
        -overwrite_reply {TRUE}
See Also
- set_hsm_params
 - create_job_project