TCPIP_IPV4_SelectSourceInterface Function
C
TCPIP_NET_HANDLE TCPIP_IPV4_SelectSourceInterface(
TCPIP_NET_HANDLE netH,
const IPV4_ADDR* pDestAddress,
IPV4_ADDR* pSrcAddress,
bool srcSet
);
Description
Updates the pSrcAddress and returns the needed interface, if successful:
if srcSet == 1 and netH != 0, the function will not change anything
if srcSet == 1 and netH == 0, the call will never fail it will use whatever value in pSrcAddress (even 0) and will try to come up with an appropriate interface
if srcSet == 0 and netH == 0, it will use the destination address
if srcSet == 0 and netH != 0, it will use the address of that interface
Preconditions
netH has to be valid (if non-0).
Parameters
| Parameters | Description |
|---|---|
| netH | Network interface handle. |
| pDestAddress | Pointer to destination address. |
| pSrcAddress | Pointer to source address. |
| srcSet | Boolean; true if address pointed by pSrcAddress is valid. |
Returns
A valid interface - If it succeeds and a valid source interface selected.
0 - Interface selection failed.
Remarks
None.