| Macros | |
| TCPIP_IPV4_FRAGMENT_MAX_NUMBER | Upper limit for the number of fragments in a fragmented stream This also imposes a limit on how large a packet could be depending on the MTU and fragmentations that occur If more fragments received for a certain stream, the stream will be discarded |
| TCPIP_IPV4_FRAGMENT_MAX_STREAMS | Upper limit for the number of fragmented streams that could be handled simultaneously |
| TCPIP_IPV4_FRAGMENT_TIMEOUT | Initial fragment timeout, in seconds Timer Lower Bound (RFC 791) The RFC states this value to be 15 seconds |
| TCPIP_IPV4_FRAGMENTATION | If 1, enable IPv4 fragmentation processing, RX + TX If 0 (default), IPv4 fragmentation not supported |
| TCPIP_IPV4_TASK_TICK_RATE | The IP task processing rate: number of milliseconds to generate an IP tick. This is the tick that advances the IP state machine. The default value is around 30 milliseconds. The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained The value cannot be lower than the TCPIP_STACK_TICK_RATE. The IP state machine tick is used only when fragmentation is enabled. |
| IP_CONFIG_H | This is macro IP_CONFIG_H. |
| TCPIP_IPV4_EXTERN_PACKET_PROCESS | This setting enables/disables the processing of the RX packets by an external handler The user of the IPv4 can register an external function to process the incoming packets If true, the functionality is built in and could be used by the application If false, the functionality does not exist and the generated code is slightly smaller |
| Functions | |
| TCPIP_IPV4_PacketGetDestAddress | Returns the IPv4 destination address associated with a TCPIP_MAC_PACKET |
| TCPIP_IPV4_PacketGetSourceAddress | Returns the IPv4 source address associated with a TCPIP_MAC_PACKET |
| TCPIP_IPV4_PacketTransmit | Transmits an IPV4 packet over the network. |
| TCPIP_IPV4_SelectSourceInterface | Selects a source address and an interface based on the IPv4 destination address |
| TCPIP_IPV4_PacketFilterClear | Clears the IPV4 packet filters |
| TCPIP_IPV4_PacketFilterSet | Sets the IPV4 packet filters |
| TCPIP_IPV4_Task | Standard TCP/IP stack module task function. |
| TCPIP_IPV4_MacPacketTransmit | Transmits a fully constructed MAC packet over the network. |
| TCPIP_IPV4_PacketAlloc | Allocates an IPv4 packet for transmission over the network. |
| TCPIP_IPV4_PacketFormatTx | Formats an IPV4 packet and makes it ready for transmission. |
| TCPIP_IPV4_PacketOptionFieldSet | Helper to set an IPv4 packet option field. |
| TCPIP_IPV4_PacketOptionGet | Helper to get the options that a IPv4 receive packet has. |
| TCPIP_IPV4_PacketOptionListGet | Helper to get the options that a IPv4 receive packet has. |
| TCPIP_IPV4_IsFragmentationEnabled | Helper to get the IPv4 fragmentation support. |
| TCPIP_IPV4_MaxDatagramDataSizeGet | Helper to get the maximum datagream data size (MDDS) on a specific interface. |
| TCPIP_IPV4_PacketHandlerDeregister | Deregisters a previously registered packet handler. |
| TCPIP_IPV4_PacketHandlerRegister | Sets a new packet processing handler. |
| Data Types and Constants | |
| IPV4_HEADER_TYPE | List of supported protocols. |
| IPV4_PACKET | IPv4 packet structure. |
| TCPIP_IPV4_FILTER_TYPE | List of supported IPv4 packet filters. |
| TCPIP_IPV4_MODULE_CONFIG | Initialization parameters supported by IPv4 |
| IPV4_FRAGMENT_INFO | Structure of an IPv4 fragment info. |
| IPV4_OPTION_FIELD | Structure of an IPv4 option. |
| IPV4_TYPE_OF_SERVICE | Structure of an IPv4 type of service field. |
| TCPIP_IPV4_OPTION_DCPT | Structure describing the options for an IPv4 packet |
| TCPIP_IPV4_OPTION_TYPE | List of supported IPv4 options |
| TCPIP_IPV4_PACKET_PARAMS | IPv4 packet formatting parameters |
| TCPIP_IPV4_PACKET_HANDLER | Pointer to a function(handler) that will get called to process an incoming IPv4 packet. |
| TCPIP_IPV4_PROCESS_HANDLE | Defines a IPv4 packet processing handle. |