TCPIP_IPV4_MaxDatagramDataSizeGet Function
C
int TCPIP_IPV4_MaxDatagramDataSizeGet(
TCPIP_NET_HANDLE netH
);
Description
This function is a helper to allow retrieving the MDDS on the specified interface.
Preconditions
IPv4 properly initialized. Interface properly initialized.
Parameters
| Parameters | Description |
|---|---|
| netH | Handle of the interface. |
Returns
The maximum datagram data size that can be transported on the selected interface.
0 - Invalid interface specified.
Remarks
None.