TCPIP_IPV4_FILTER_TYPE Enumeration
C
typedef enum {
TCPIP_IPV4_FILTER_NONE = 0x00,
TCPIP_IPV4_FILTER_UNICAST = 0x01,
TCPIP_IPV4_FILTER_BROADCAST = 0x02,
TCPIP_IPV4_FILTER_MULTICAST = 0x04
} TCPIP_IPV4_FILTER_TYPE;
Description
IPv4 packet filters.
This is the list of the packet filters that are supported by this IPv4 implementation. There are 3 types of IPv4 packets currently supported:
unicast
broadcast
multicast
An IPV4 packet is accepted if the filter corresponding to the packet type is not set.
Parameters
| Parameters | Description |
|---|---|
| TCPIP_IPV4_FILTER_NONE = 0x00 | No packet filter active. All packets are accepted. |
| TCPIP_IPV4_FILTER_UNICAST = 0x01 | Unicast packets will be filtered out. |
| TCPIP_IPV4_FILTER_BROADCAST = 0x02 | Broadcast packets will be filtered out. |
| TCPIP_IPV4_FILTER_MULTICAST = 0x04 | Multicast packets will be filtered out. |
Returns
None.
Remarks
Multiple filters can be set.
If no filter is set, all packets are accepted; this is the default case.