IPV4_FRAGMENT_INFO Union
C
typedef union {
uint16_t val;
struct {
uint16_t fragOffset : 13;
uint16_t MF : 1;
uint16_t DF : 1;
uint16_t reserved : 1;
}
} IPV4_FRAGMENT_INFO;
Description
IPv4 packet fragment definition.
This is the structure of an IPv4 fragment info in the IPv4 header.
Parameters
| Parameters | Description |
|---|---|
| uint16_t fragOffset : 13; | Fragment offset. |
| uint16_t MF : 1; | More fragments. |
| uint16_t DF : 1; | Don't fragment. |
Returns
None.
Remarks
None.