TCPIP_IPV4_PacketFilterSet Function
C
TCPIP_IPV4_FILTER_TYPE TCPIP_IPV4_PacketFilterSet(
TCPIP_IPV4_FILTER_TYPE filtType
);
Description
The function will set the IPv4 packet filters. The filters that are present in the mask will be set. Other filters won't be touched.
Preconditions
filtType - valid IPv4 filter IPv4 properly initialized.
Parameters
| Parameters | Description |
|---|---|
| filtType | Packet filter mask to set. |
Returns
The current value of the IPV4 packet filters after this mask was applied.
Remarks
None.