IPV4_TYPE_OF_SERVICE Union
C
typedef union {
uint8_t val;
struct {
uint8_t reserved : 2;
uint8_t reliability : 1;
uint8_t throughput : 1;
uint8_t delay : 1;
uint8_t precedence : 3;
}
} IPV4_TYPE_OF_SERVICE;
Description
IPv4 type of service definition.
This is the structure of an IPv4 type of service header field.
Parameters
| Parameters | Description |
|---|---|
| uint8_t reserved : 2; | Not used. |
| uint8_t reliability : 1; | Reliability settings: normal/high. |
| uint8_t throughput : 1; | Throughput settings: normal/high. |
| uint8_t delay : 1; | Delay settings: normal/low. |
| uint8_t precedence : 3; | Precedence; one of TCPIP_IPV4_PRECEDENCE_ values. |
Returns
None.
Remarks
None.