TCPIP_UDP_DestinationPortSet Function
C
bool TCPIP_UDP_DestinationPortSet(UDP_SOCKET s, UDP_PORT remotePort); Returns
true - Indicates success
false - Indicates an invalid socket
Description
This function sets the destination port, which allows changing the destination port dynamically.
Remarks
The destination remote port will always be changed, even if remotePort == 0. It will not change the UDP_OPTION_STRICT_PORT on the socket.
Preconditions
UDP initialized UDP socket should have been opened with TCPIP_UDP_ServerOpen/TCPIP_UDP_ClientOpen. hUDP - valid socket
Parameters
| Parameters | Description |
|---|---|
| hUDP | the UDP socket |
| remotePort | destination port to use |