TCPIP_UDP_ClientOpen Function
C
UDP_SOCKET TCPIP_UDP_ClientOpen(IP_ADDRESS_TYPE addType, UDP_PORT remotePort, IP_MULTI_ADDRESS* remoteAddress); Returns
INVALID_SOCKET - No sockets of the specified type were available to be opened.
A UDP_SOCKET handle - Save this handle and use it when calling all other UDP APIs.
Description
Provides a unified method for opening UDP client sockets.
Remarks
Sockets and user threads protection For efficiency reasons, there is NO PROTECTION for each individual API call except to Open and Close sockets! What it means is that:
the user application should close all its sockets before issuing a stack/if down command The stack manager takes care of the internally used sockets
A socket can NOT be used concurrently from multiple threads! It's ok to pass a socket from one thread to another as long as there's is no access from more than one thread at a time
Preconditions
UDP is initialized.
Parameters
| Parameters | Description |
|---|---|
| IP_ADDRESS_TYPE | addType The type of address being used. Example: IP_ADDRESS_TYPE_IPV4 or IP_ADDRESS_TYPE_IPV6. It can also be IP_ADDRESS_TYPE_ANY if the type of the socket will be specified later (using TCPIP_UDP_Bind, TCPIP_UDP_RemoteBind). |
| UDP_PORT | remotePort The remote UDP port to which a connection should be made. The local port for client sockets will be automatically picked by the UDP module. |
| IP_MULTI_ADDRESS* | remoteAddress The remote address to connect to. Not used if addType == IP_ADDRESS_TYPE_ANY. Can be NULL if later set by a call to TCPIP_UDP_RemoteBind. |