TCPIP_UDP_SourceIPAddressSet Function
C
bool TCPIP_UDP_SourceIPAddressSet(UDP_SOCKET hUDP, IP_ADDRESS_TYPE addType, IP_MULTI_ADDRESS* localAddress); Returns
true - Indicates success
false - Indicates failure:
invalid socket
invalid socket address type
unspecified localAddress
Description
This function sets the IP source address, which allows changing the source P address dynamically.
Remarks
The call will fail if localAddress is 0. The source IP address will not be changed.
Preconditions
UDP initialized UDP socket should have been opened with TCPIP_UDP_ServerOpen/TCPIP_UDP_ClientOpen. hUDP - valid socket localAddress - valid address pointer
Parameters
| Parameters | Description |
|---|---|
| hUDP | the UDP socket |
| addType | Type of address: IPv4/IPv6 |
| localAddress | pointer to an address to use |