TCPIP_UDP_TxOffsetSet Function
C
bool TCPIP_UDP_TxOffsetSet(UDP_SOCKET hUDP, uint16_t wOffset, bool relative); Returns
true - if the offset was valid and the write pointer has been moved
false - if the offset was not valid
Description
This function allows the write location within the TX buffer to be specified. Future calls to TCPIP_UDP_Put, TCPIP_UDP_ArrayPut, TCPIP_UDP_StringPut, etc will write data from the indicated location.
Preconditions
UDP socket should have been opened with TCPIP_UDP_ServerOpen/TCPIP_UDP_ClientOpen. hUDP - valid socket
Parameters
| Parameters | Description |
|---|---|
| hUDP | UDP socket handle |
| wOffset | Offset in the UDP packet data payload to move the write pointer. |
| relative | if true, the wOffset is added to the current write pointer. else the wOffset is from the beginning of the UDP buffer |